STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

A comparison of C compilers for the STM8

Posted on June 15, 2016 at 10:18A comparison of the 4 most important C implementations for the STM8 can be found at:http://colecovision.eu/stm8/compilers.shtml It uses the current (mid 2016) versions of all 4 compilers. Only aspects of the C impleme...

>> how do i measure machine clock [STM8S103K3 : STVD+COSMIC_C]

Posted on August 11, 2016 at 16:41First, i,m sorry for my bad in English.How do i measure machine clock [STM8S103K3 : STVD+COSMIC_C]now.. i config TIM1..  ENABLEbut CNT bit of TIM1 is strange..value's value are..  1000 , next line 24001 ,next line 6...

ADC Sleep Mode

Posted on August 09, 2016 at 01:34Hi,I am wondering if there is a sleep mode for the ADC for the STM8S003f3 processor.I want the processor to sleep until ADC_CSR_EOC = 1 or sleep while ADC_CSR_EOC = 0I did see a WEI but I believe it is only for the ...

ghan by Associate
  • 699 Views
  • 0 replies
  • 0 kudos

Build ERROR.. Execution from ram [stm8s + Cosmic_C]

Posted on July 30, 2016 at 01:54I'm sorry for my bad in English.[STVD + COSMIC_C : STM8S103K3]I want to use prototype function which need EXECUTION_FROM_RAM.after i  build.. It ERROR..!!help me please..  T_T!// ------------------------ below.. is st...

UART2 of STM8S not working with HSI clock

Posted on July 14, 2016 at 14:09Hi I am prashant. I am using stm8s microcontroller with uart2 . First thing is that when i am using uart explicitly without configure the clock to 16Mhz ( HSI clock), uart throwing the garbage values. Secondly when i ...

sh by Associate
  • 688 Views
  • 0 replies
  • 0 kudos

STM8 Visual programmer

Posted on June 17, 2016 at 15:40Hi all,I am working on STM8 bootloader configuration.Can anyone please provide a link for STM8 visual programmer software and how to use it for unlocking the unlocking the STM8 bootloader.Thanks in advanceAmit Kumaram...

amitkrv22 by Associate II
  • 1505 Views
  • 2 replies
  • 0 kudos

STM8/128 Board CAN messages pending in mailbox

Posted on July 01, 2016 at 13:17my fCPU is16MHz. In order to get 500K baudrate, I have programmed as follows: CAN_SynJumpWidth = CAN_SynJumpWidth_1TimeQuantum;  CAN_BitSeg1 = CAN_BitSeg1_8TimeQuantum ;  CAN_BitSeg2 = CAN_BitSeg2_7TimeQuantum;  CAN_P...

rr by Associate
  • 854 Views
  • 0 replies
  • 0 kudos