STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART communication using STM8L discovery

Posted on August 23, 2015 at 08:54Hi,I am new to use STM8L controller.I am just trying to put Simple character on UART using STM8L discovery board.But I am failed to do this.Following is my code for this.void main(void){        u8 Data = 'N';       ...

Using Eclipse and STVD with Cosmic

Posted on September 29, 2016 at 15:03Due to the CDT debugging issue this is a fair workaround for productivity (convenience due to Eclipse, issue tracking, git handling, doxygen (eclox) etc.)Google always helps, so I gathered all info I found and te...

hjs by Associate II
  • 1232 Views
  • 0 replies
  • 0 kudos

Getting Cosmic C setup with STVD

Posted on September 28, 2016 at 15:36I've downloaded STVD, installed it, Downloaded Cosmic C, installed it and downloaded en.stsw-stm8069.zip (standard peripheral library) Now. I cannot for the life of me get this thing working. I opened the .stw pr...

wfd by Associate II
  • 878 Views
  • 1 replies
  • 0 kudos

Simulation STM8AL3188 in HyperLynx

Posted on September 28, 2016 at 12:54Hi Dear, I Need IBIS Model STM8AL3188 to Simulation it in the HyperLynx ? IS there it ? Thanks for attention.  

no ST-Link detected *sometimes

Posted on September 23, 2016 at 19:24I'm using the ST-Link V2 as a programmer repeatedly.  Sometimes it returns no ST-Link detected when I try to program.  Unplugging the device then plugging it in again solves the problem. When its in this state, I...

Code example STM8L152C6

Posted on August 30, 2016 at 10:07Hi, I'm trying to find some code examples I can run though using the STM8L152C6 micro. I'm new to this so I wanted some proven code I can step though and make sure I understand all of the commands, can anyone point ...

STM8 Linker: text size overflow ... just in Release ... not in Debug

Posted on April 08, 2016 at 17:04Hello everyone!Currently I'm switching from an Atmel ATTiny to a STM8 microcontroller and so I'm evaluating different IDEs and compilers. I started with a combination of the ST Visual Development and the COSMIC STM8 ...

cr by Associate
  • 1990 Views
  • 2 replies
  • 1 kudos

ADC scan conversion timing issue, channel order

Posted on August 22, 2016 at 19:12Greetings,    I am using an STM8L and I'm trying to use the ADC.  I'm trying to continuously sample 2 channels and use DMA to transfer the results.  Everything is working fine with one exception.  After about 10 sam...

Power Consumption with Input NOT at Rail

Posted on February 02, 2016 at 23:22I am using the STM8S103K3.  The data specifies power consumption only with all inputs at the rail voltage.  Also the data sheet says to ''turn off schmitt input'' on adc input to save power.  These things imply th...

Measure Time duration between high and low pulse

Posted on August 13, 2016 at 12:55I am working on STM8S003K3 microcontroller. I need to calculate time duration between two pulses. One high pulse (1) and another low pulse (0). The pulses will be created using switch. Approximate time duration woul...

anuj by Associate II
  • 577 Views
  • 0 replies
  • 0 kudos