STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST Visual Develop Compile Error

Posted on October 14, 2016 at 09:02Hi, I used the ST Visual Develop with Cosmic STM8 free tools with no limits version to compile a C program. However, some errors were shown, ''&sharperror clnk debug\stm8 gerenal io program.lkf:1 can't open file de...

smwong by Associate
  • 660 Views
  • 0 replies
  • 0 kudos

I2C problem when use STM8AF6223 - Eeprom24C128

Posted on October 13, 2016 at 08:53 Hi All, When I use STM8AF6223 read data from eeprom 24C128,I can't poll RXNE flag. This is my code for Read Eeprom: uint8_t Read_EEPROM(uint8_t EepAddr,uint8_t RegAddr) { uint8_t data=0; /* check ...

0690X00000604yTQAQ.png

DAC for stm8l151G6U6

Posted on March 20, 2013 at 05:19Hi all, I used DAC and it OK on stm8l151C6T6,  this is 48pin MCU. But now i change to 28pin DAC.It not work:     CLK_PeripheralClockConfig(CLK_Peripheral_DAC, ENABLE);     DAC_DeInit();     DAC_Init(DAC_Channel_1, DA...

np1 by Associate II
  • 747 Views
  • 3 replies
  • 0 kudos

Maximal toggling frequency of STM8

Posted on October 07, 2016 at 15:06Hi,I have just started with STM8 and would like to found the fastest toggling method.Currently I have best result with following code: while (1) {#pragma asm push A pushw X ld A, #1 // toggle with pin D0 ldw X, #0x...

How to Establish LIN communication between STM8AL and STM8AF

Posted on October 06, 2016 at 07:47Hello all,               I am new to LIN protocol, stuck in establishing LIN communication between STM8AF and STM8AL boards. I am referring to example code found in STM forum for LIN communication. I have downloade...

Through-Hole Microcontroller with Evaluation Tool

Posted on October 05, 2016 at 20:17Hi, I'm working on a project that needs a microcontroller to produce a control signal for an analog audio effect. The microcontroller I choose needs the following requirements:-Through-Hole / DIP package-At least 4...

epalaima by Associate II
  • 1238 Views
  • 0 replies
  • 0 kudos

STM8S003 registry access

Posted on October 05, 2016 at 15:26Our company as an electronic engineering company is willing to use your products specifically STM8S003.For more than 12 years we have used Atmel products and have lots of experiences on it.Beginning with your STM8S...

Cannot compile with Cosmic

Posted on February 26, 2016 at 03:20Hi,I'm trying to use the Cosmic 32K compiler in ST Visual develop and having created a completely new project with no additional code in, I can't compile it. I can't compile using Idea either.My error is:&sharperr...

harris by Associate II
  • 1249 Views
  • 2 replies
  • 0 kudos

UART communication using STM8L discovery

Posted on August 23, 2015 at 08:54Hi,I am new to use STM8L controller.I am just trying to put Simple character on UART using STM8L discovery board.But I am failed to do this.Following is my code for this.void main(void){        u8 Data = 'N';       ...

Using Eclipse and STVD with Cosmic

Posted on September 29, 2016 at 15:03Due to the CDT debugging issue this is a fair workaround for productivity (convenience due to Eclipse, issue tracking, git handling, doxygen (eclox) etc.)Google always helps, so I gathered all info I found and te...

hjs by Associate II
  • 1208 Views
  • 0 replies
  • 0 kudos