STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hello, I had developed one application using STVD

Posted on April 14, 2017 at 14:29void Menu(void){    if(KeypadStatus == Button_ADD)    {        Display_Filling_Constant(&CONF[0],DISPLAY_1,5);        Display_Filling_Constant(&MENU[0],DISPLAY_2,5);        Display_Filling_Constant(&BLANK[0],DISPLAY_...

EEprom writing issue

Posted on April 12, 2017 at 10:17Hello,I am trying to write value 7 to eeprom data memory area. My code is below../* MAIN.C file *  * Copyright (c) 2002-2005 STMicroelectronics */#include 'STM8S003F3P.h' unsigned int *ptr=(unsigned int *)0X4000; mai...

Resolved! STM8 _block_cksum161

Posted on April 12, 2017 at 11:01i used _blockcksum160 then we increase code size 32K to 64Kdepends on code size increased;we changed memory model +modsl0 to modsl.We changed library list libislo.sm8;libmo.sm8 to libisl.sm8;libm.sm8We changed startu...

__ckdesc__

Posted on April 13, 2017 at 10:07can you decribe __ckdesc__?Can i set these adress?

Data Memory read Issue

Posted on April 12, 2017 at 09:07The original post was too long to process during our migration. Please click on the attachment to read the original post.

stm8s003f3p6 eeprom program

Posted on April 12, 2017 at 06:26Hello,Does any one have  stm8s003f3p6 eep-rom read and write example code in stvd. How do I assign  dataeeprom  address directly to a pointer variable. unsigned  int *ptr=(unsigned int *)0x4047;   is this OK?? Thanks...

stm8s003f3 does not answer

Posted on April 09, 2017 at 08:00Hello every bodyI am new in stm8s003f3  i use iar code limited and stlink/v2I read error swim 30006 and i can't correct it Please help me#swim-error

_stext not defined

Posted on April 06, 2017 at 16:20Hi. I change memory model and libraries for code larger than 64K. The error receive after linking: #error clnk Debug\canli.lkf:1 symbol __stext not defined (Debug\stm8l_stl_startup.o ) The command: 'clnk -l'C:\Progra...

When I am trying to upload simple gpio code I am getting the following errors..can anyone help me please An error occurred while retrieving GDI features: gdi-error [40201]: Can't access configuration database Couldn't find STM8S003F3 in the list of

Posted on March 21, 2017 at 13:28&sharpinclude <iostm8s003f3.h>&sharpinclude <intrinsics.h>int main(){ // // Initialise Port D. // PD_ODR = 0; // All pins are turned off. PD_DDR_DDR4 = 1; // Port D, bit 4 is output. PD_CR1_C14 = 1; // Pin is set to ...