STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is it the strange CPU instruction generated by SDCC?

Hello everyone.SLCC generated a strange instruction similar to JRF, represented as .byte 0x21 pseudo-instruction. Can anyone explain what this is? A code snippet is provided in the attachment. The compiler options are as follows: -mstm8 --out-fmt-elf...

I request sample from estore, but when i get to the shipping page, no matter how i fill out anything, the cointue button cant work and cant pass to next page,so i gave up requesting sample ,so pls st send me free sample stm8s103k3t6, thanks.

I request sample from estore, but when i get to the shipping page, no matter how i fill out anything, the cointue button cant work and cant pass to next page,so i gave up requesting sample ,so pls st send me free sample stm8s103k3t6, thanks.

STM8AF6223A how to pass ASIL B certification?

Hi All​The customer want to design STM8AF6223A for automotive application, it is have to pass ASIL B certification, but I had confirm ST website(as below hyperlink), the third party website has expired, how to get more detailed information?Thanks.​ht...

Felix1 by Associate II
  • 578 Views
  • 0 replies
  • 0 kudos

About STM8S003 be reset continoustly

Hello everyone, I have got a problem but I can't resolve it.I made a project read NMEA string from UART and show it to OLED 128x64 (I2C interface) with STM8s003F3P6. everything is OK when I tried to get GPS strings from UART and store them variable ,...

qloi by Associate
  • 542 Views
  • 0 replies
  • 0 kudos

Can I add 30 minutes delay using Timer or RTC in STM8L051F3

I am currently trying to put STM8 in sleep mode after 30 minutes if no activity is observed on I2C. I am able to use timer4 to get a delay in ms upto 1 secs but I am unable to get delay in minutes. Do I need to use RTC for this? If so can someone ...

BUG: HSE_Value should be HSE_VALUE in stm8s.h

This bug is several years old and should really be fixed.In stm8s.h, the following line ...#if !defined HSE_Value... should (obviously!) be ...#if !defined HSE_VALUE... in order to allow HSE_VALUE to be defined on the command-line.I just found out th...

pacman by Associate III
  • 1974 Views
  • 4 replies
  • 0 kudos

STVD not handling EEPROM data correctly

I have an issue when I am using STVD with Cosmic to write a value to EEPROM and read it back.Example code :/* MAIN.C file *  * Copyright (c) 2002-2005 STMicroelectronics */#include "stm8s.h"#include "stm8s_flash.h"@eeprom unsigned char eeValue;unsign...

BCowa by Associate II
  • 1004 Views
  • 2 replies
  • 0 kudos