2019-10-10 3:27 PM
/* MAIN.C file
*
* Copyright (c) 2002-2005 STMicroelectronics
*/
#include <iostm8l.h>
#include <stdio.h>
#include <string.h>
#include <stdlib.h>
#include <stdint.h>
#include "defs.h"
unsigned int count = 0;
unsigned int pwm_duty = 0x0000;
void TIM2_SetCompare1(uint16_t Compare)
{
TIM2_CCR1H = (uint8_t)(Compare >> 8);
TIM2_CCR1L = (uint8_t)(Compare);
}
void delay(unsigned long dd)
{
unsigned long i;
for (i=0;i<dd;i++) nop();
}
@svlreg @interrupt void TIM2(void)
{
PC_ODR ^= 0x80;
TIM2_SR1 &= ~2;
}
main()
{
CLK_DIVR = 0x00; // Set the frequency to 16Mhz
CLK_PCKENR1 = 0x01; // clock for timer2
PC_DDR = 0x80; // direction output for led
PC_CR1 = 0x80; // fast push pull mode for led
PB_DDR = 0x01;
PB_CR1 = 0x01;
PB_CR2 = 0x00;
PB_ODR = 0x01;
TIM2_PSCR = 0x07;// 125000
TIM2_ARRH = 0x03;// 50000
TIM2_ARRL = 0xe8;
TIM2_CCMR1 = 0x60;
TIM2_CCER1 = 0x01;
TIM2_CR1 = 0x01;
while(1)
{
for(pwm_duty = 0; pwm_duty <500 ; pwm_duty += 25)
{
TIM2_SetCompare1(pwm_duty);
delay(pwm_duty);
}
for(pwm_duty =500; pwm_duty > 0; pwm_duty -= 25)
{
TIM2_SetCompare1(pwm_duty);
delay(pwm_duty);
}
}
}