cancel
Showing results for 
Search instead for 
Did you mean: 

Can someone give me any link for bare metal programming of LCD in stm8l discovery. Any help would be greatly appreciated

VSrin
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Vyacheslav Azarov
Associate III

Standard Peripheral Library have a good example relative to LCD. Details of LCD control you can extract from corresponding source file of this library. See application note also. https://www.st.com/content/ccc/resource/technical/document/application_note/0d/99/cb/9c/dc/73/42/52/CD00257713.pdf/files/CD00257713.pdf/jcr:content/translations/en.CD00257713.pdf

VSrin
Associate II

I have a quick question? I use ST visual develop and I could not see my variables getting incremented if I set the variables as static.

#include <iostm8l.h>

#include <stdio.h>

#include <string.h>

#include <stdlib.h>

#include <stdint.h>

#include <math.h>

#include "defs.h"

static int click = 0;

void delay(unsigned long dd)

{

  unsigned long i;

  for (i=0;i<dd;i++) nop(); 

}

void RTC(void)

{

unsigned long j = 0;

PE_ODR |= 0x80; // led indication for reset 

if( click == 2) // reset module

{

click = 0;

 PC_ODR &= ~(1<<3); //pc3 in place of push button - turn it off here

 for(j = 0;j<20;j++)

 {

  delay(_250ms_); // 4.3 seconds in real

 }

}

if(click == 1) // on module

{

click++;

PC_ODR &= ~(1<<3); //turn it off

for(j = 0;j<8;j++)

 {

delay(_250ms_); // wait

 }

}

if (click == 0) // off module

{

PC_ODR &= ~(1<<3); //turn it off

click++;

 for(j = 0;j<8;j++)

 {

delay(_250ms_); // wait

 }

  PC_ODR |= (1<<3); // turn it on

 for(j = 0;j<8;j++)

 {

delay(_250ms_); // wait

 }

 PC_ODR &= ~(1<<3); //turn it off

 for(j = 0;j<8;j++)

 {

delay(_250ms_); // wait

 }

}

RTC_ISR2=0x00; // clear interrupt flags

}

void SetupTimers(void)

{

CLK_CRTCR=0x04; // use iternal LSI/1 clock @ ~38KHz

 RTC_WPR=0xCA;

RTC_WPR=0x53;

RTC_CR2=0x00; // disable wakeup timer for register update

while(!(RTC_ISR1 & 0x04));

  RTC_CR1=0x04; // set 1hz clk

RTC_WUTRH=0x00; // change here for time change

RTC_WUTRL=0x78; //2 min timer

RTC_CR3=0x00; 

RTC_CR2=0x44; // turn on timer and interrupt

RTC_WPR=0xFF; // lock the device

}

main()

{

CLK_DIVR = 0x00; // Set the frequency to 16Mhz

CLK_PCKENR2 = 0x07; // clock for timer1

 PC_DDR = 0x08; //direction input for push button

PC_CR1 = 0x08; //floating input pc3

PE_DDR = 0x80; // direction output for led

 PE_CR1 = 0x80; // fast push pull mode

SetupTimers();

_asm("rim\n"); // enable interrupt

while(1)

{

PC_ODR |= (1<<3); // turn it on

PE_ODR &= ~(0x80);

}

}

VSrin
Associate II

The static click remains 0 all the time

Vyacheslav Azarov
Associate III

STVD MCU simulator have some limitation of functionality. As example you must stimulate interrupts requests manually. To make the program understandable, best use the definitions from the Standard Peripheral Library.