cancel
Showing results for 
Search instead for 
Did you mean: 

After the installation of STVD-STM8, Active ST, version : 42.0.0 software. I am facing the license problem and compiling error.

PAgra.1
Associate

When i choose the option of "ST Assembler linker" in C Compiler it compiles the code but the code is not burn in MCU successfully. And when STM8 cosmic is selected there is an error while compiling

" The command: "cxstm8 +mods0 +debug -pxp -no -pp -l -iinc -i"C:\Program Files\COSMIC\FSE_Compilers\CXSTM8\Hstm8" -clDebug\ -coDebug\ main.c" has failed, the returned value is: 1

exit code=1.

".

License problem is "flexnet license finder" which asks for the license. Which i do not have?

Kindly, revert back

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0