STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is the proper code for STM8S External Interrupt?

Being new to STM8 development, I'm having a problem getting the external interrupt to work. There are many bits and pieces of external interrupt code I've found on the internet, but I haven't found a definitive piece of code that works as expected. H...

JKain.1 by Associate
  • 1462 Views
  • 0 replies
  • 0 kudos

After the installation of STVD-STM8, Active ST, version : 42.0.0 software. I am facing the license problem and compiling error.

When i choose the option of "ST Assembler linker" in C Compiler it compiles the code but the code is not burn in MCU successfully. And when STM8 cosmic is selected there is an error while compiling " The command: "cxstm8 +mods0 +debug -pxp -no -pp -l...

PAgra.1 by Associate
  • 686 Views
  • 0 replies
  • 1 kudos

communicate stm8s with mpu6050

Hello to all. I am completely new to stm8. I want to communicate stm8s003 with mpu6050 6-axis gyroscope and accelerometer sensor through i2c. Can anyone help me how to code it in st visual develop?Sorry for my bad English

oebra.1 by Associate
  • 863 Views
  • 1 replies
  • 0 kudos

STM8S001J EEPROM PROBLEMS

HelloI'm using STM8S001j in my projectthe Project is simply an output on PB4 and output on PD6I needed to store in the EEPROM data every time the input is getting low I noticed that some times the data is recorded and some times not I monitored the E...

AAraf.1 by Associate
  • 741 Views
  • 1 replies
  • 0 kudos

Reliability of STM8S internal MVR...

Because I don't find related information elsewhere (datasheet, application notes, etc.) I would ask it there.​So, I have famous W1209 thermostat board with Nuvoton MCU, which I'm replace by an STM8S103F3.For proper operation it is needed to place an ...

VPant.1 by Associate
  • 556 Views
  • 0 replies
  • 0 kudos

CRC for CAN frame in STM8AF5286

I am using STM8AF5286 for one of my design. I am using CAN port for data transmission. I am using standard ST library for CAN communication. I don't see any 16-bit CRC calculation included in CAN_Transmit function of CAN driver function. Neither I se...

PPate.1 by Associate III
  • 637 Views
  • 0 replies
  • 0 kudos