i have made another project for the ads1115 integration for stm8l052c6 ..with peripheral clock and all
#include "stm8l15x.h"
#include "stm8l15x_clk.h"
#include "stm8l15x_i2c.h"
#include <stdio.h>
// ADS1115 I2C address
#define ADS1115_ADDRESS 0x48
// ADS1115 configuration registers
#define CONFIG_REG_ADDR 0x01
#define AIN0_CONFIG 0xC3 // Example configuration for AIN0
uint8_t i;
uint16_t adcValue=0;
// Function prototypes
void I2C_Init(I2C_TypeDef* I2Cx, uint32_t OutputClockFrequency, uint16_t OwnAddress,
I2C_Mode_TypeDef I2C_Mode, I2C_DutyCycle_TypeDef I2C_DutyCycle,
I2C_Ack_TypeDef I2C_Ack, I2C_AcknowledgedAddress_TypeDef I2C_AcknowledgedAddress);
void I2C_Cmd(I2C_TypeDef* I2Cx, FunctionalState NewState);
void I2C_GenerateSTART(I2C_TypeDef* I2Cx, FunctionalState NewState);
void I2C_GenerateSTOP(I2C_TypeDef* I2Cx, FunctionalState NewState);
void I2C_Send7bitAddress(I2C_TypeDef* I2Cx, uint8_t Address, I2C_Direction_TypeDef I2C_Direction);
void I2C_SendData(I2C_TypeDef* I2Cx, uint8_t Data);
uint8_t I2C_ReceiveData(I2C_TypeDef* I2Cx);
// Delay function
void delay(uint16_t ms) {
// Assuming a 16 MHz clock frequency
uint16_t cycles = (uint16_t)(16000 * ms);
while (cycles--) {
// Do nothing
}
}
void Clock_Init(void) {
CLK_DeInit();
CLK_LSICmd(DISABLE); // Disable Low-Speed Internal clock
CLK_HSICmd(ENABLE); // Enable High-Speed Internal clock
while (CLK_GetFlagStatus(CLK_FLAG_HSIRDY) == FALSE);
CLK_SYSCLKSourceConfig(CLK_SYSCLKSource_HSI);
// Enable peripheral clocks
CLK_PeripheralClockConfig(CLK_Peripheral_I2C1, ENABLE);
CLK_PeripheralClockConfig(CLK_Peripheral_USART1, ENABLE);
}
/*void USART_Configuration(void) {
// UART initialization
USART_Init(USART1, (uint32_t)19200, USART_WordLength_8b,
USART_StopBits_1, USART_Parity_No, (USART_Mode_TypeDef)(USART_Mode_Tx|USART_Mode_Rx));
}*/
void I2C_Configuration(void) {
// I2C initialization
I2C_Init(I2C1, 100000, 0, I2C_Mode_I2C, I2C_DutyCycle_2, I2C_Ack_Enable, I2C_AcknowledgedAddress_7bit);
}
void ADS1115_Configuration(void) {
// Initialize clock
Clock_Init();
// Initialize I2C
I2C_Configuration();
// Start I2C communication
while (I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY));
I2C_GenerateSTART(I2C1, ENABLE);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));
// Send ADS1115 address for write operation
I2C_Send7bitAddress(I2C1, (ADS1115_ADDRESS << 1 & 0xFE), I2C_Direction_Transmitter);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));
// Send configuration register address
I2C_SendData(I2C1, CONFIG_REG_ADDR);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
// Send configuration data
I2C_SendData(I2C1, AIN0_CONFIG);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
// End I2C communication
I2C_GenerateSTOP(I2C1, ENABLE);
while (I2C_GetFlagStatus(I2C1, I2C_FLAG_STOPF));
}
uint16_t ADS1115_Read_A0(void) {
uint8_t data[2] = {0};
// Start I2C communication
while (I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY));
I2C_GenerateSTART(I2C1, ENABLE);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));
// Send ADS1115 address for write operation
I2C_Send7bitAddress(I2C1, (ADS1115_ADDRESS << 1& 0xFE), I2C_Direction_Transmitter);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));
// Send register address to read from (Config register)
I2C_SendData(I2C1, CONFIG_REG_ADDR);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_TRANSMITTED));
// Repeated start
I2C_GenerateSTART(I2C1, ENABLE);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_MODE_SELECT));
// Send ADS1115 address for read operation
I2C_Send7bitAddress(I2C1, (ADS1115_ADDRESS << 1| 0x01), I2C_Direction_Receiver);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_RECEIVER_MODE_SELECTED));
// Receive data
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED));
data[0] = I2C_ReceiveData(I2C1);
// Acknowledge disable
I2C_AcknowledgeConfig(I2C1, DISABLE);
// Generate stop condition
I2C_GenerateSTOP(I2C1, ENABLE);
// Receive data
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_BYTE_RECEIVED));
data[1] = I2C_ReceiveData(I2C1);
return (data[0] << | data[1];
}
void GPIO_Configuration(void) {
// Remap USART1 to PA2 (TX) and PA3 (RX)
GPIO_DeInit(GPIOA);
SYSCFG_REMAPPinConfig(REMAP_Pin_USART1TxRxPortA, ENABLE);
// Configure PA2 (TX) as alternate function push-pull
GPIO_Init(GPIOA, GPIO_Pin_2, GPIO_Mode_Out_PP_Low_Slow);
// Configure PA3 (RX) as input floating
GPIO_Init(GPIOA, GPIO_Pin_3, GPIO_Mode_In_FL_No_IT);
}
int main(void) {
enableInterrupts();
// Call ADS1115 configuration function
ADS1115_Configuration();
// Your main code here
// USART_Configuration();
while (1) {
// Read value from A0 using ADS1115
adcValue = ADS1115_Read_A0();
// Your code to process the ADC value
/*char buffer[50]; // Adjust the array size based on the expected length of your values
sprintf(buffer, "ADC Value: %u", adcValue);
i = 0;
while (buffer[i] != '\0') {
USART_SendData8(USART1, buffer[i++]);
while (!USART_GetFlagStatus(USART1, USART_FLAG_TC)); */ // Wait for transmission to complete
// Introduce a delay if necessary
delay(1000);
}
}
in this code also stops aftr the i2c is started , when the address is being send to slave
I2C_Send7bitAddress(I2C1, (ADS1115_ADDRESS << 1 & 0xFE), I2C_Direction_Transmitter);
while (!I2C_CheckEvent(I2C1, I2C_EVENT_MASTER_TRANSMITTER_MODE_SELECTED));
have any suggetion
also can anyone provide a i2c scanner code for stm8l052c6 mcu