cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H562RIT6 is not programmed

Farhad13651
Associate II

Hi

I have designed a header board for the STM32H562RIT6 microcontroller, but no matter how hard I try, I can't program it! The wiring is as follows. Please guide me on how to program this microcontroller. If there are any tips or specific instructions for programming this microcontroller, I would appreciate your help.

WIRING ( SIMILAR TO AN5711 PAGE 36 ) :

All VDD and VDDA pins → connect to 3.3V

All VSS and VSSA pins → connect to GND

BOOT0 → connect to GND through a 10kΩ resistor

RESET → connect to GND through a 100nF capacitor

Connect the two VCAP pins together, and connect each pin to a 2.2µF capacitor

PROGRAMMER : ST-LINK V2 ( 3.3V , GND , SWDIO , SWCLK )

1 ACCEPTED SOLUTION

Accepted Solutions

Hello,


@Farhad13651 wrote:

The software is STM32 ST-LINK Utility, and I have placed Roshamatic in the "Youst" folder.


No. ST-LINK Utility is an old tool and doesn't support that device. You need to use STM32CubeProgrammer instead.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
mÆŽALLEm
ST Employee

Hello @Farhad13651 and welcome to the community,

1- Insufficient information. Better to share your schematics.

2- What tools are you using? STLINK (genuine or not) with STM32CubeProgrammer or CubeIDE?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.

The software is STM32 ST-LINK Utility, and I have placed shamatic 

The software is STM32 ST-LINK Utility, and I have placed schematic.

Hello,


@Farhad13651 wrote:

The software is STM32 ST-LINK Utility, and I have placed Roshamatic in the "Youst" folder.


No. ST-LINK Utility is an old tool and doesn't support that device. You need to use STM32CubeProgrammer instead.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.