cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 / STM32G491 What is the difference in external loader?

LehuW
Associate III

Hi,

I can't get the external loader to work in STM32G491.
For the test, I replaced the bodies of the Init()/Erase()/Write() function with LED blinking. I did this to check if the functions are called correctly. For debugging, I used STM32_Programmer_CLI to check the writing of single bytes.

If I try to write the STM32F429 I get this log.

19:50:54:384 ------------------------------------------------------------------- 19:50:54:384 STM32CubeProgrammer v2.9.0 19:50:54:384 ------------------------------------------------------------------- 19:50:54:384 19:50:54:388 Log output file: !log.txt 19:50:54:390 Command line: -log !log.txt 19:50:54:390 19:50:54:395 Operation [2]: -vb 3 19:50:54:406 Operation [3]: -c port=swd freq=500 reset=HWrst 19:50:54:447 ST-LINK SN : 55FF67065065565040110987 19:50:54:450 ST-LINK FW : V2J45S0 19:50:54:453 Board : -- 19:50:54:455 Voltage : 2.92V 19:50:54:481 SWD freq : 480 KHz 19:50:54:484 Connect mode: Under Reset 19:50:54:486 Reset mode : Hardware reset 19:50:54:491 Device ID : 0x419 19:50:54:495 Revision ID : Rev Y 19:50:54:530 Reading data... 19:50:54:536 r ap 0 @0x40023C14 0x00000004 bytes Data 0x0FFFAAED 19:50:54:539 Reading data... 19:50:54:542 r ap 0 @0x1FFF7A22 0x00000004 bytes Data 0xFFFF0800 19:50:54:545 Database: Config 0 is active. 19:50:54:547 flash loader C:/STM32CubeProgrammer/bin/FlashLoader/0x419.stldr is loaded 19:50:54:552 Reading data... 19:50:54:557 r ap 0 @0x40023C14 0x00000004 bytes Data 0x0FFFAAED 19:50:54:559 Reading data... 19:50:54:563 r ap 0 @0x1FFF7A22 0x00000004 bytes Data 0xFFFF0800 19:50:54:565 Database: Config 0 is active. 19:50:54:567 Device name : STM32F42xxx/F43xxx 19:50:54:572 Reading data... 19:50:54:574 r ap 0 @0x1FFF7A22 0x00000004 bytes Data 0xFFFF0800 19:50:54:577 Flash size : 2 MBytes 19:50:54:579 Device type : MCU 19:50:54:582 Device CPU : Cortex-M4 19:50:54:585 BL Version : 0x70 19:50:54:590 19:50:54:591 Operation [4]: -el "c:\STM32CubeProgrammer\bin\ExternalLoader\F429_EXL.stldr" 19:50:54:603 external loader c:\STM32CubeProgrammer\bin\ExternalLoader\F429_EXL.stldr is loaded 19:50:54:614 Operation [5]: -w8 0x90000000 0xAA 0xBB 0x55 0xCC 0x11 0x22 0x33 19:50:54:627 Downloading 8-bit data... 19:50:54:631 Buffer program... 19:50:54:637 halt ap 0 19:50:54:637 w ap 0 reg 15 PC (0x20000000) 19:50:54:642 w ap 0 reg 17 MSP (0x20000500) 19:50:54:647 w ap 0 reg 16 xPSR (0x01000000) 19:50:54:669 w ap 0 @0x20008360 : 0x00000200 bytes, Data 0x00000000... 19:50:54:674 w ap 0 @0x20000000 : 0x00000004 bytes, Data 0x0000BE00... 19:50:55:684 w ap 0 @0x20000004 : 0x00007F28 bytes, Data 0x00000000... 19:50:55:698 Loader write range... 19:50:55:700 w ap 0 @0x20008360 : 0x00000008 bytes, Data 0xCC55BBAA... 19:50:55:705 W B1 in RAM @0x20008360 size 0x00000008 : 0005ms 19:50:55:708 Init flashloader... 19:50:55:711 halt ap 0 19:50:55:714 w ap 0 reg 0 R0 0x00000001 19:50:55:722 w ap 0 reg 1 R1 0x00000000 19:50:55:743 w ap 0 reg 2 R2 0x00000000 19:50:55:751 w ap 0 reg 3 R3 0x00000000 19:50:55:757 w ap 0 reg 4 R4 0x00000000 19:50:55:760 w ap 0 reg 5 R5 0x00000000 19:50:55:765 w ap 0 reg 6 R6 0x00000000 19:50:55:770 w ap 0 reg 7 R7 0x00000000 19:50:55:774 w ap 0 reg 8 R8 0x00000000 19:50:55:777 w ap 0 reg 9 R9 0x00000000 19:50:55:781 w ap 0 reg 10 R10 0x00000000 19:50:55:785 w ap 0 reg 11 R11 0x00000000 19:50:55:789 w ap 0 reg 12 R12 0x00000000 19:50:55:793 w ap 0 reg 13 SP 0x00000000 19:50:55:796 w ap 0 reg 14 LR 0x20000001 19:50:55:801 w ap 0 reg 15 PC 0x20000985 19:50:55:805 w ap 0 reg 16 xPSR 0x01000000 19:50:55:808 w ap 0 reg 17 MSP 0x20008328 19:50:55:813 w ap 0 reg 18 PSP 0x00000000 19:50:55:817 run ap 0 19:50:57:748 halt ap 0 19:50:57:754 r ap 0 reg 0 R0 0x00000001 19:50:57:760 w ap 0 reg 0 R0 0x90000000 19:50:57:765 w ap 0 reg 1 R1 0x00000008 19:50:57:770 w ap 0 reg 2 R2 0x20008360 19:50:57:774 w ap 0 reg 3 R3 0x00000002 19:50:57:779 w ap 0 reg 4 R4 0x00000000 19:50:57:784 w ap 0 reg 5 R5 0x00000000 19:50:57:788 w ap 0 reg 6 R6 0x00000000 19:50:57:792 w ap 0 reg 7 R7 0x00000000 19:50:57:796 w ap 0 reg 8 R8 0x00000000 19:50:57:804 w ap 0 reg 9 R9 0x00000000 19:50:57:809 w ap 0 reg 10 R10 0x00000000 19:50:57:814 w ap 0 reg 11 R11 0x00000000 19:50:57:819 w ap 0 reg 12 R12 0x00000000 19:50:57:823 w ap 0 reg 13 SP 0x00000000 19:50:57:827 w ap 0 reg 14 LR 0x20000001 19:50:57:831 w ap 0 reg 15 PC 0x20000A25 19:50:57:837 w ap 0 reg 16 xPSR 0x01000000 19:50:57:841 w ap 0 reg 17 MSP 0x20008328 19:50:57:845 w ap 0 reg 18 PSP 0x00000000 19:50:57:848 run ap 0 19:50:58:966 r ap 0 reg 0 R0 0x00000001 19:50:58:970 Write elapsed time: 3270ms 19:50:58:971 Reading data...
View more

If I try to write the STM32G491 I get this log.

19:54:29:059 ------------------------------------------------------------------- 19:54:29:059 STM32CubeProgrammer v2.9.0 19:54:29:059 ------------------------------------------------------------------- 19:54:29:060 19:54:29:062 Log output file: !log.txt 19:54:29:065 Command line: -log !log.txt 19:54:29:065 19:54:29:070 Operation [2]: -vb 3 19:54:29:082 Operation [3]: -c port=swd freq=500 reset=HWrst 19:54:29:176 ST-LINK SN : 50FF71064977535538100587 19:54:29:181 ST-LINK FW : V2J45S7 19:54:29:184 Board : -- 19:54:29:186 Voltage : 3.22V 19:54:29:213 SWD freq : 480 KHz 19:54:29:216 Connect mode: Under Reset 19:54:29:217 Reset mode : Hardware reset 19:54:29:222 Device ID : 0x479 19:54:29:228 Revision ID : Rev Z 19:54:29:246 Reading data... 19:54:29:249 r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0200 19:54:29:251 Database: Config 0 is active. 19:54:29:255 flash loader C:/STM32CubeProgrammer/bin/FlashLoader/0x479.stldr is loaded 19:54:29:262 Reading data... 19:54:29:265 r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0200 19:54:29:267 Database: Config 0 is active. 19:54:29:270 Device name : STM32G491xx 19:54:29:271 Reading data... 19:54:29:273 r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0200 19:54:29:277 Flash size : 512 KBytes 19:54:29:279 Device type : MCU 19:54:29:280 Device CPU : Cortex-M4 19:54:29:283 BL Version : 0xD2 19:54:29:287 19:54:29:288 Operation [4]: -el "c:\STM32CubeProgrammer\bin\ExternalLoader\F429_EXL.stldr" 19:54:29:299 external loader c:\STM32CubeProgrammer\bin\ExternalLoader\F429_EXL.stldr is loaded 19:54:29:312 Operation [5]: -w8 0x90000000 0xAA 0xBB 0x55 0xCC 0x11 0x22 0x33 19:54:29:322 Downloading 8-bit data... 19:54:29:326 Buffer program... 19:54:29:333 halt ap 0 19:54:29:334 w ap 0 reg 15 PC (0x20000000) 19:54:29:339 w ap 0 reg 17 MSP (0x20000500) 19:54:29:346 w ap 0 reg 16 xPSR (0x01000000) 19:54:29:351 Loader write range...
View more


What does this mean?
Does STM32_Programmer not loading the external loader into RAM?
Does the processor not executing the run command?
Does the processor have interrupts disabled ?


I am using STM32CubeIDE Version: 1.17.0

I need external loader for TouchGfx in configuration W25Q128VS (QSPI mode) + STM32G491RE

 

1 ACCEPTED SOLUTION

Accepted Solutions
LehuW
Associate III

I reduced the used memory and everything works properly.

Every tutorial I've seen shows to uncheck 'Discard unused sections' ( to keep the compiler from removing unused code). But this results in including a lot of functions that are not needed at all and the size of the resulting file is large. In my case it was about 30kB of used memory (112kB total RAM).

To solve the problem, I checked the 'Discard unused sections' option and called the Init()/Erase()/Write() finctions from the main program so that they would not be optimized. Now the used memory is 15kB RAM. This change caused the external loader to work correctly.

Conclusions:
There is some limitation on the size of the external loader file, but I did not find such information in any manual.
CubeProgrammer does not give any information why it does not want to load the external loader into RAM.
Maybe there is some other reason, but so far I don't know it.

View solution in original post

5 REPLIES 5

Does it load MT25QL512ABB_STM32G474E-EVAL.stldr ?

https://community.st.com/t5/stm32-mcus-embedded-software/stm32g491-does-not-start-from-ram-in-debug-mode-external-loader/td-p/755895

Your configuration

PA3:AF10 CLK

PA2:AF10 NCS

PB1:AF10 IO0

PB0:AF10 IO1

PA7:AF10 IO2

PA6:AF10 IO3

Do you have a serial port?

PD2 GPIO LED ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you for the reply.

>> Does it load MT25QL512ABB_STM32G474E-EVAL.stldr ?
Yes. Log attached below.

 

QSPI config exactly as you wrote.

 

>> Do you have a serial port?

I have UART3 PB10:TX, PB11:RX  (and RS485 USART1; PC4:TX; PC5:RX, PA12:DE).

 

>> PD2 GPIO LED ?

Yes.

 

Below log from loading MT25QL512ABB_STM32G474E-EVAL.stldr

22:01:39:919 ------------------------------------------------------------------- 22:01:39:919 STM32CubeProgrammer v2.9.0 22:01:39:919 ------------------------------------------------------------------- 22:01:39:919 22:01:39:924 Log output file: !log.txt 22:01:39:929 Command line: -log !log.txt 22:01:39:929 22:01:39:934 Operation [2]: -vb 3 22:01:39:947 Operation [3]: -c port=swd freq=500 reset=HWrst 22:01:39:990 ST-LINK SN : 50FF71064977535538100587 22:01:39:994 ST-LINK FW : V2J45S7 22:01:39:998 Board : -- 22:01:40:000 Voltage : 3.22V 22:01:40:027 SWD freq : 480 KHz 22:01:40:033 Connect mode: Under Reset 22:01:40:035 Reset mode : Hardware reset 22:01:40:040 Device ID : 0x479 22:01:40:044 Revision ID : Rev Z 22:01:40:059 Reading data... 22:01:40:067 r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0200 22:01:40:071 Database: Config 0 is active. 22:01:40:076 flash loader C:/STM32CubeProgrammer/bin/FlashLoader/0x479.stldr is loaded 22:01:40:083 Reading data... 22:01:40:084 r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0200 22:01:40:089 Database: Config 0 is active. 22:01:40:094 Device name : STM32G491xx 22:01:40:098 Reading data... 22:01:40:103 r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0200 22:01:40:108 Flash size : 512 KBytes 22:01:40:109 Device type : MCU 22:01:40:116 Device CPU : Cortex-M4 22:01:40:123 BL Version : 0xD2 22:01:40:129 22:01:40:133 Operation [4]: -el "c:\STM32CubeProgrammer\bin\ExternalLoader\MT25QL512ABB_STM32G474E-EVAL.stldr" 22:01:40:144 external loader c:\STM32CubeProgrammer\bin\ExternalLoader\MT25QL512ABB_STM32G474E-EVAL.stldr is loaded 22:01:40:156 Operation [5]: -w8 0x90000000 0xAA 0xBB 0x55 0xCC 0x11 0x22 0x33 22:01:40:167 Downloading 8-bit data... 22:01:40:173 Buffer program... 22:01:40:184 halt ap 0 22:01:40:185 w ap 0 reg 15 PC (0x20000000) 22:01:40:193 w ap 0 reg 17 MSP (0x20000500) 22:01:40:199 w ap 0 reg 16 xPSR (0x01000000) 22:01:40:221 w ap 0 @0x200036A0 : 0x00000200 bytes, Data 0x00000000... 22:01:40:225 w ap 0 @0x20000000 : 0x00000004 bytes, Data 0x0000BE00... 22:01:40:640 w ap 0 @0x20000004 : 0x00003274 bytes, Data 0x20000001... 22:01:40:658 Loader write range... 22:01:40:661 w ap 0 @0x200036A0 : 0x00000008 bytes, Data 0xCC55BBAA... 22:01:40:665 W B1 in RAM @0x200036A0 size 0x00000008 : 0005ms 22:01:40:670 Init flashloader... 22:01:40:672 halt ap 0 22:01:40:676 w ap 0 reg 0 R0 0x00000001 22:01:40:683 w ap 0 reg 1 R1 0x00000000 22:01:40:687 w ap 0 reg 2 R2 0x00000000 22:01:40:691 w ap 0 reg 3 R3 0x00000000 22:01:40:696 w ap 0 reg 4 R4 0x00000000 22:01:40:701 w ap 0 reg 5 R5 0x00000000 22:01:40:706 w ap 0 reg 6 R6 0x00000000 22:01:40:710 w ap 0 reg 7 R7 0x00000000 22:01:40:715 w ap 0 reg 8 R8 0x00000000 22:01:40:719 w ap 0 reg 9 R9 0x00000000 22:01:40:723 w ap 0 reg 10 R10 0x00000000 22:01:40:726 w ap 0 reg 11 R11 0x00000000 22:01:40:731 w ap 0 reg 12 R12 0x00000000 22:01:40:734 w ap 0 reg 13 SP 0x00000000 22:01:40:738 w ap 0 reg 14 LR 0x20000001 22:01:40:742 w ap 0 reg 15 PC 0x2000000F 22:01:40:750 w ap 0 reg 16 xPSR 0x01000000 22:01:40:768 w ap 0 reg 17 MSP 0x20003674 22:01:40:774 w ap 0 reg 18 PSP 0x00000000 22:01:40:776 run ap 0 22:01:40:785 halt ap 0 22:01:40:788 r ap 0 reg 0 R0 0x00000001 22:01:40:795 w ap 0 reg 0 R0 0x90000000 22:01:40:799 w ap 0 reg 1 R1 0x00000008 22:01:40:803 w ap 0 reg 2 R2 0x200036A0 22:01:40:807 w ap 0 reg 3 R3 0x00000002 22:01:40:812 w ap 0 reg 4 R4 0x00000000 22:01:40:817 w ap 0 reg 5 R5 0x00000000 22:01:40:822 w ap 0 reg 6 R6 0x00000000 22:01:40:827 w ap 0 reg 7 R7 0x00000000 22:01:40:834 w ap 0 reg 8 R8 0x00000000 22:01:40:839 w ap 0 reg 9 R9 0x00000000 22:01:40:843 w ap 0 reg 10 R10 0x00000000 22:01:40:848 w ap 0 reg 11 R11 0x00000000 22:01:40:851 w ap 0 reg 12 R12 0x00000000 22:01:40:856 w ap 0 reg 13 SP 0x00000000 22:01:40:861 w ap 0 reg 14 LR 0x20000001 22:01:40:866 w ap 0 reg 15 PC 0x20000065 22:01:40:870 w ap 0 reg 16 xPSR 0x01000000 22:01:40:874 w ap 0 reg 17 MSP 0x20003674 22:01:40:881 w ap 0 reg 18 PSP 0x00000000 22:01:40:883 run ap 0 22:01:40:893 r ap 0 reg 0 R0 0x00000001 22:01:40:897 Write elapsed time: 0236ms 22:01:40:899 Reading data... 22:01:40:910 halt ap 0 22:01:40:914 w ap 0 reg 15 PC (0x20000000) 22:01:40:919 w ap 0 reg 17 MSP (0x20000500) 22:01:40:922 w ap 0 reg 16 xPSR (0x01000000) 22:01:40:944 w ap 0 @0x200036A0 : 0x00000200 bytes, Data 0x00000000... 22:01:40:950 w ap 0 @0x20000000 : 0x00000004 bytes, Data 0x0000BE00... 22:01:41:359 w ap 0 @0x20000004 : 0x00003274 bytes, Data 0x20000001... 22:01:41:380 halt ap 0 22:01:41:381 w ap 0 reg 15 PC (0x20000000) 22:01:41:387 w ap 0 reg 17 MSP (0x20000500) 22:01:41:393 w ap 0 reg 16 xPSR (0x01000000) 22:01:41:415 w ap 0 @0x200036A0 : 0x00000200 bytes, Data 0x00000000... 22:01:41:421 w ap 0 @0x20000000 : 0x00000004 bytes, Data 0x0000BE00... 22:01:41:830 w ap 0 @0x20000004 : 0x00003274 bytes, Data 0x20000001... 22:01:41:844 Init flashloader... 22:01:41:847 halt ap 0 22:01:41:851 w ap 0 reg 0 R0 0x00000000 22:01:41:855 w ap 0 reg 1 R1 0x00000000 22:01:41:860 w ap 0 reg 2 R2 0x00000000 22:01:41:865 w ap 0 reg 3 R3 0x00000000 22:01:41:868 w ap 0 reg 4 R4 0x00000000 22:01:41:873 w ap 0 reg 5 R5 0x00000000 22:01:41:876 w ap 0 reg 6 R6 0x00000000 22:01:41:881 w ap 0 reg 7 R7 0x00000000 22:01:41:885 w ap 0 reg 8 R8 0x00000000 22:01:41:888 w ap 0 reg 9 R9 0x00000000 22:01:41:898 w ap 0 reg 10 R10 0x00000000 22:01:41:904 w ap 0 reg 11 R11 0x00000000 22:01:41:908 w ap 0 reg 12 R12 0x00000000 22:01:41:914 w ap 0 reg 13 SP 0x00000000 22:01:41:919 w ap 0 reg 14 LR 0x20000001 22:01:41:923 w ap 0 reg 15 PC 0x2000000F 22:01:41:930 w ap 0 reg 16 xPSR 0x01000000 22:01:41:934 w ap 0 reg 17 MSP 0x20003674 22:01:41:938 w ap 0 reg 18 PSP 0x00000000 22:01:41:940 run ap 0 22:01:41:954 halt ap 0 22:01:41:958 r ap 0 reg 0 R0 0x00000001 22:01:41:965 r ap 0 @0x90000000 0x00000001 bytes Data 0x00000000 22:01:41:973 halt ap 0 22:01:41:979 w ap 0 reg 15 PC (0x20000000) 22:01:41:983 w ap 0 reg 17 MSP (0x20000500) 22:01:41:987 w ap 0 reg 16 xPSR (0x01000000) 22:01:41:992 22:01:41:994 Error: failed to read memory 22:01:42:001 Error: Downloading 8-bit data failed... If it's a Flash memory, it may be not erased or protected
View more

 

Looks to be an older version of STM32 Cube Programmer, but interesting that it loads the .STLDR to RAM

@Aziz BRIGUI any thoughts to why the stock STLDR for the G474 EVAL might load whilst others don't

Any sanity or size checks on the .STLDR, alignment? Any diagnostic output that Cube Programmer could provide about an issue or inability to load?

 

 

The NUCLEO-G491RE might be a workable proxy, but not a board I have to hand. Some of your pins also don't map to the header, but PB10/PB11 might be workable, or I might have to remap ARD_D0/ARD_D1

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

I have done the test on the NUCLEO-G491RE. The result is the same.

LehuW
Associate III

I reduced the used memory and everything works properly.

Every tutorial I've seen shows to uncheck 'Discard unused sections' ( to keep the compiler from removing unused code). But this results in including a lot of functions that are not needed at all and the size of the resulting file is large. In my case it was about 30kB of used memory (112kB total RAM).

To solve the problem, I checked the 'Discard unused sections' option and called the Init()/Erase()/Write() finctions from the main program so that they would not be optimized. Now the used memory is 15kB RAM. This change caused the external loader to work correctly.

Conclusions:
There is some limitation on the size of the external loader file, but I did not find such information in any manual.
CubeProgrammer does not give any information why it does not want to load the external loader into RAM.
Maybe there is some other reason, but so far I don't know it.