Skip to main content
Associate
August 11, 2023
Question

STM32F030F4P6 programming

  • August 11, 2023
  • 7 replies
  • 3025 views

Hi, I have a problem about upload program. I make size photocell with STM32F030F4P6 MCU. After I set hardware and software, I can not upload programming to MCU. I try to upload programming with ST-LİNK V2. And writing problem at console. Error is that ;

Target no device found

Error in initializing ST-LINK device.
Reason: No device found on target.

What can I do?I control connection pinout. Coming 3.3V and connection pinouts is correct. Please Can you give advice?

Thank you.

This topic has been closed for replies.

7 replies

Peter BENSCH
ST Technical Moderator
August 11, 2023

Welcome @NİHAT_EEE, to the community!

Is your ST-LINK/V2 in a colourful metal box?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate
August 11, 2023

Yes, it is colourful metal box.

AScha.3
Super User
August 11, 2023

do you have any other STM board or discovery board , to test : connect and working with CubeProgrammer ?

 

If you feel a post has answered your question, please click on " Best Answer ".
Associate
August 11, 2023

Yes, I try cube programmer and ST-link V2 at breadboard. İt is working both of them.

AScha.3
Super User
August 11, 2023

so on your breadboard its ok, you can program the cpu ?

then you have some bad or wrong connection to your target board. 

boot0 low ?

connect mode : " software reset "

 

If you feel a post has answered your question, please click on " Best Answer ".
Visitor II
July 22, 2025

Niekedy je potrebné pripojiť aj NRST programator s doskou.