2020-05-18 8:29 AM
Hello,
DFU is not working in STM32Cube Programmer, I can see the connected board in device manager under universal serial bus controllers, please your advise.
Thanks
2020-05-18 1:33 PM
Does it show up in device manager as a DFU device? Show a screenshot. It's not in that mode by default, you need to start the bootloader with USB enabled and nothing else talking to the chip.
2020-05-18 1:39 PM
Hello @AAmer.1
which board do you use ?
Best regards,
Nesrine
2020-05-19 2:42 AM
Hello Nesrine,
I have our own board.
BR
2020-05-19 2:59 AM
Hello @AAmer.1
So, it is necessary to know if your Board contains a bootloader or not.
Best regards,
Nesrine
2020-05-19 3:03 AM
this is the reason why I'm trying to connect to it, I need to flash it with bootloader.
2020-05-19 3:04 AM
It is necessary to check the boot on the system memory.
2020-05-19 3:09 AM
yes I knew, the boot are correct, strange.
2020-05-19 7:40 AM
No it appears as USB serial converter
2020-05-19 7:47 AM
Hello @AAmer.1
I think that the problem is on the user's own board not on the Cubeprogrammer.
Best regards,
Nesrine