2025-08-24 3:17 AM
Hi everyone,
I try to connect to my NUCLEO board (NUCLEO-L476RG) via STM32CubeProgrammer but I receive the following error message:
I reinstalled the STM32CubeProgrammer but nothing changed. I used to write my program to the MCU flash several times using Copy/Paste .bin file directly to the following storage before:
but I am not enable to program the MCU via STM32CubeProgrammer. Even I am not able to use Copy/Paste to program the MCU anymore.
This is my NUCLEO development board: (NUCLEO-L476RG)
Does anyone have any solution please?
Thanks
Peyman
2025-08-24 6:26 AM
Does the correct voltage show up?
Try holding BOOT0 during reset, then connecting.
If you remove connections to other things, does it work?