2024-11-04 9:29 AM
I just get a STM32F401CCU6 board (a real one) but now when I try to connect my board on STM32CubeProgrammer the application crahses... and when is unplug my board the application work again fine...
It also look like my board is stuck in bootloader mode ( only the red led lights up)
I don't know if someone could help me...
Thank you
2024-11-04 9:43 AM
2024-11-04 10:25 AM
As I said, it is a STM32F401CCU6 board (a stmicroelectronic)
ANd for the version of CubeProgrammer :
2024-11-04 10:40 AM
And why don't you use the current version, 2.17?
2024-11-04 10:45 AM
Okay I will try with the latest version
Thanks for your help
2024-11-04 11:01 AM
Okay now I am running on the 2.17 version but there is still the same problem
2024-11-05 1:08 AM - edited 2024-11-05 1:08 AM
@Totouan wrote:As I said, it is a STM32F401CCU6 board (a stmicroelectronic)
That's just the chip - not the board.
Is it a Discovery board? a Nucleo board? an EV board? other?
2024-11-05 2:22 AM
I assume it's BlackPill. I think the problem is not related to the board/chip at all. CubeProgrammer frequently installs incorrectly. Then it tries (sometimes even with success) to display some strange error messages about missing components or refuses to execute some actions. That's probably the case here.
2024-11-05 2:44 AM
2024-11-05 3:45 AM
Sorry i didn't understood, here is the link from the product i bought : https://www.amazon.fr/dp/B0CLD5FG62?ref=ppx_yo2ov_dt_b_fed_asin_title