2024-07-11 10:38 PM
Hello,
On STM32CubeProgrammer CLI v2.15.0 the below command was working fine and erasing the EEPROM of my STM32L151.
STM32_Programmer_CLI.exe -c port=SWD -e ed1
> Erase sector(s) ...
> Existing specified sectors are erased successfully
> Protected sectors are not erased
With the new v2.17.0 the same command give me the following error:
Error: You are performing erase operation but you are missing to indicate the sectors you want to erase, Please refer to the help for more details on the Erase command parametres.
I checked the documentation and release notes and I did not find any changes in the CLI about my MPU.
What's wrong?
2024-07-15 03:21 AM
Hello @scachemaille,
Thank you for bringing this issue to our attention, I've submitted an internal ticket for resolution.
Internal ticket number: 186569 (This is an internal tracking number and is not accessible or usable by customers)
I will keep you updated on any progress.
Thanks,
Amine.