cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeProgrammer can see the USB device in DFU mode, but cannot connect.

ANgo.1
Associate

 set the device to DFU mode through USB. It shows up in device manager. STM32CubeProgrammer shows the port USB1, and show serial number.  I can select the address 0x8000000 size 0x40 and click read and see the result. But when I click on the Connect, it just hangs and fail. On the FW side, which function it calls to connect? I need t debug why it cannot connect.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Houda GHABRI
ST Employee

Hi @ANgo.1​ ,

Can you please tell me which MCU and board are you using?

regards,

Houda