cancel
Showing results for 
Search instead for 
Did you mean: 

ST-Link/V2 CLI asking user to press return

hans86
Associate III

This might have already been asked in the past, is there a way to not having to press return after programming a file with (old) ST-LINK CLI Utility?

I am using the command line version which works fine but before the program runs ST-LINK stop and waits for the user to press return, then the program runs and ST-LINK terminates.

If you run this from a third party application the required CR is annoying.

Here is what happens, you run the programmer:

 

 

H:\STM32\node>ST-Link_CLI -c SWD UR Hrst -p node.hex -run
STM32 ST-LINK CLI v3.6.0.0
STM32 ST-LINK Command Line Interface

ST-LINK SN: 5200371004300132594E514E
ST-LINK Firmware version: V2J45S7
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 3.3 V
Connection mode: Connect Under Reset
Reset mode: Hardware reset
Device ID: 0x450
Device flash Size: 2048 Kbytes
Device family: STM32H7xx

Loading file...
Flash Programming:
  File : H:/STM32/build/Debug/node.hex
  Address : 0x08000000
Memory programming...
█████████████████████████████████████████████████▒ 99%
Ram programming...
██████████████████████████████████████████████████ 100%
Memory programmed in 1s and 609ms.
Programming Complete.

run application to exit

 

 

The program now wait, when the user presses return the program continues and terminate:

 

 

Application started.

H:\STM32\node>

 

 

I found no option under the help menu to just run without me having to press return.

Note that I cannot use the STM32_Programmer_CLI programmer as it does not work with a cloned ST-Link/V2 programmer which I bought (unknowingly),

Thanks,
Hans.

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Use echo to pipe an enter to the command:

H:\STM32\node>echo | ST-Link_CLI -c SWD UR Hrst -p node.hex -run

 

 Depending on how you're running this from the third party application, might need some configuring, but it will work on a straight command line.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

4 REPLIES 4
Andrew Neil
Super User

@hans86 wrote:

I cannot use the STM32_Programmer_CLI programmer as it does not work with a cloned ST-Link/V2 programmer which I bought (unknowingly)


A genuine ST-Link/V2 is only about £20.

Or break one off a cheap (under £9) Nucleo board ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi Andrew,

Thanks for replying, yes you are of course correct, however, money is not the issue. I just wondered if there is some old... I mean experienced ST user who fixed this issue which is quicker than me ordering another board or programmer,

Regards,
Hans.

TDK
Super User

Use echo to pipe an enter to the command:

H:\STM32\node>echo | ST-Link_CLI -c SWD UR Hrst -p node.hex -run

 

 Depending on how you're running this from the third party application, might need some configuring, but it will work on a straight command line.

If you feel a post has answered your question, please click "Accept as Solution".
hans86
Associate III

Hi TDK,

Great solution!

Thanks,
Hans