2025-03-22 11:12 AM
Hello
As I am trying to connect the STM32N6570-DK board on the STM32CubeProgrammer, initially the STM32CubeProgrammer recognises my device as in the following picture:
When I press Connect on the STM32CubeProgrammer I get a
warning: Connection to device 0x486 is lost
as in the following picture:
and then an error that says Data read fail
as in the following picture:
I am using a MacBook Air M3, 2024, but even on windows (running on a virtual machine) I get the same error on the STM32CubeProgrammer windows version.
Is there a way to overcome this issue? What could be the cause?
Thank you
2026-03-28 9:19 AM
Yes.
And even when using an external SWD programmer (via MIPI20 connector, i believe) I still get the same error. I've tried with three different PCs now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.