2023-02-10 08:56 AM
2023-02-11 10:28 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter
2023-02-10 12:38 PM
The command file for Windows STM32Bootloader.bat can be found after the installation of STM32CubeProg in the installation path, i.e. normally in
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\Drivers\DFU_Driver
By the way, when working with STM32CubeIDE, it is strongly recommended not to change the target path of the STM32CubeProg, so that the tools of STM32CubeIDE can launch the programmer.
Does it answer your question?
Regards
/Peter
2023-02-10 03:46 PM
Hi Peter: This is exactly what I was looking for. Many thanks!!
2023-02-11 10:28 AM
Great!
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards
/Peter