2021-11-19 8:17 PM
Hi,
I have a STM32G030F6P6 connected to an STLink. I cannot upload at least an LED toggle code to the chip. I get the following messages in the CubeProgrammer. And I get "Cannot insert all breakpoints" error in the CUBE IDE.
I double triple checked my voltages. They are 3.3V. But still the messages from the Cube Programmer shows as 2.93V. Can you please comment on this and help me.
09:30:41 : STM32CubeProgrammer API v2.8.0
09:30:41 : ST-LINK error (DEV_CONNECT_ERR)
09:31:01 : ST-LINK SN : 34FF6D064155303923251357
09:31:01 : ST-LINK FW : V2J38S7
09:31:01 : Board : --
09:31:01 : Voltage : 2.93V
09:31:01 : SWD freq : 4000 KHz
09:31:01 : Connect mode: Normal
09:31:01 : Reset mode : Hardware reset
09:31:01 : Device ID : 0x466
09:31:01 : Revision ID : Rev 1.1
09:31:02 : UPLOADING OPTION BYTES DATA ...
09:31:02 : Bank : 0x00
09:31:02 : Address : 0x40022020
09:31:02 : Size : 112 Bytes
09:31:02 : UPLOADING ...
09:31:02 : Size : 1024 Bytes
09:31:02 : Address : 0x8000000
09:31:02 : Read progress:
09:31:02 : Data read successfully
09:31:02 : Time elapsed during the read operation is: 00:00:00.008
09:31:04 : Memory Programming ...
09:31:04 : Opening and parsing file: DryBox Test.hex
09:31:04 : File : DryBox Test.hex
09:31:04 : Size : 5316 Bytes
09:31:04 : Address : 0x08000000
09:31:04 : Erasing memory corresponding to segment 0:
09:31:04 : Erasing internal memory sectors [0 2]
09:31:04 : Error: failed to erase memory
09:31:04 : Error: failed to erase memory
09:31:04 : Error: Unable to get core ID
09:31:04 : Error: Unable to get core ID
09:31:04 : Warning: Connection to device 0x466 is lost
09:31:05 : Disconnected from device.
09:31:05 : ST-LINK error (DEV_CONNECT_ERR)
09:31:15 : Error: Connection to target must be established before performing file download operation.
09:31:15 : Error: Connection to target must be established before performing the execute command.
09:31:18 : ST-LINK SN : 34FF6D064155303923251357
09:31:18 : ST-LINK FW : V2J38S7
2021-11-20 4:32 AM
Hello, this processor is on your board or bought from some site?
I got many of these cheap board with processor locked with a bad cfg word, no idea why they do this. Symptom are unreadable processor and failure on erase like your report. From cube programmer read CFG register and look at value.
From your log programmer report Hardware reset, is reset pin connected? If not change to software reset and retry.
If this doesn't solve, connect reset pin then launch cube programmer and do a full chip erase. After that processor is unlocked and you can access.
2022-03-21 2:19 AM
I have the same issue with an stm32g030j6, the parts are original stm32 from trusted source.
The mcus were programmed before (no serial wire debugging pins were enabled), now when i want to programm them again i get a similar error than @Sahiru
I tried in CubeProgrammer Modes :
Power down
10:16:30:393 : STLinkUSBDriver.dll loaded
10:16:30:395 : STLinkUSBDriver.dll loaded
10:16:30:396 : ST-LINK SN : 50FF6D067788545440291967
10:16:30:396 : ST-LINK FW : V2J39S7
10:16:30:396 : Board : --
10:16:30:397 : Voltage : 3.21V
10:16:31:608 : SWD freq : 4000 KHz
10:16:31:608 : Connect mode: Power Down
10:16:31:608 : Reset mode : Hardware reset
10:16:31:614 : Device ID : 0x466
10:16:31:614 : Revision ID : Rev 1.1
10:16:31:632 : Reading data...
10:16:31:636 : r ap 0 @0x1FFF77DD 0x00000004 bytes Data 0xFF000030
10:16:31:636 : Reading data...
10:16:31:637 : r ap 0 @0x1FFF77DD 0x00000004 bytes Data 0xFF000030
10:16:31:637 : Database: Config 1 is active.
10:16:31:638 : flash loader C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin/FlashLoader/0x466.stldr is loaded
10:16:31:639 : Reading data...
10:16:31:641 : r ap 0 @0x1FFF75E0 0x00000004 bytes Data 0xFFFF0020
10:16:31:805 : UPLOADING OPTION BYTES DATA ...
10:16:31:806 : Bank : 0x00
10:16:31:806 : Address : 0x40022020
10:16:31:806 : Size : 112 Bytes
10:16:31:806 : Reading data...
10:16:31:806 : r ap 0 @0x40022020 0x00000070 bytes Data 0xDFFFE1AA
10:16:31:807 : UPLOADING OPTION BYTES DATA ...
10:16:31:807 : Bank : 0x00
10:16:31:807 : Address : 0x40022020
10:16:31:807 : Size : 112 Bytes
10:16:31:807 : Reading data...
10:16:31:807 : r ap 0 @0x40022020 0x00000070 bytes Data 0xDFFFE1AA
10:16:31:808 : UPLOADING ...
10:16:31:808 : Size : 1024 Bytes
10:16:31:808 : Address : 0x8000000
10:16:31:808 : Read progress:
10:16:31:809 : Reading data...
10:16:31:809 : r ap 0 @0x08000000 0x00000400 bytes Data 0x20002000
10:16:31:809 : Data read successfully
10:16:31:809 : Time elapsed during the read operation is: 00:00:00.006
10:16:32:786 : Error: Unable to get core ID
10:16:32:790 : Error: Unable to get core ID
10:16:32:790 : Warning: Connection to device 0x466 is lost
10:16:33:116 : Disconnected
10:16:33:117 : Disconnected from device.
10:16:33:119 : STLinkUSBDriver.dll loadedNormal/hot plug/under reset
10:34:43:880 : STLinkUSBDriver.dll loaded
10:34:43:881 : STLinkUSBDriver.dll loaded
10:34:43:882 : ST-LINK SN : 50FF6D067788545440291967
10:34:43:882 : ST-LINK FW : V2J39S7
10:34:43:883 : Board : --
10:34:43:884 : Voltage : 3.21V
10:34:43:887 : Error: No STM32 target found!
10:34:43:902 : Disconnected
2022-03-21 2:47 AM
it turned out to be defective wiring, all works for me now