cancel
Showing results for 
Search instead for 
Did you mean: 

can't update STM32 Cube Programmer

mha
Associate

Hi,

when starting STM32 Cube Programmer (W64) or checking for updates I get this message

mha_0-1697473614723.png

There is "No Proxy" set in the Proxy settings and the Windows PC has internet access (browsing www works).

Any ideas?

Thanks,

M

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12

1.
I've tried different proxy settings (both "No Proxy" and "Use System Proxy Parameters").

I clicked on check connection, and I got the green check instead of the red cross (as shown in the figure).

Check Connection - No Proxy (OK) 2023-11-18.jpg

 

Check Connection - Use System Proxy Parameters (OK) 2023-11-18.jpg

 

2.
However, when I click on software update, the connection error occurs (as shown in the figure).

Updater download - Connection error! 2023-11-18.jpg

 

------------------------
System Information:
Use VMware
DISTRIB_DESCRIPTION="Ubuntu 22.04.3 LTS" provided by osboxes.org
STM32CubeProgrammer, version 2.14.0
I've checked my network connection. The web browser can normally connected to the internet.

I've used STM32CubeProgrammer to create partitions into micro SD cards in the STM32MP157F-DK2 development board. An error occurred and the STM32CubeProgrammer stopped working (as shown in the figure, log file attached).
STM32CubeProgrammer - Error during buring 2023-11-21.jpg

 

[Problem solved] The image can be downloaded to the target board and booted successfully via STM32CubeProgrammer

 

[2023-12-15 Friday]

I got a hint from the webpage "Populate the target and boot the image."

 

Hint:
STM32CubeProgrammer v2.14.0 is recommended for ecosystem release v5.0.0
REF: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image

 

Hence, I tried to use Ecosystem v5.0.0 and chose the "FlashLayout_sdcard_stm32mp157F-dk2-optee.tsv" file in the Starter Package.
It works. The image was downloaded to the target board and booted successfully.


[2023-12-18 Monday]

I tried to use Ecosystem v5.0.0 and chose the "FlashLayout_sdcard_stm32mp157f-dk2-extensible.tsv" file in the Starter Package.
It works. The image was downloaded to the target board and booted successfully.

[問題解決] 可以燒錄 extensible - 2023-12-18.jpg

 

NOTE: [Filename inconsistancy]

The tar.gz filenames of the starter package stated in the webpages "Populate the target and boot the image" and "STM32MP1-Ecosystem-v5.0.0 Starter Package" are not the same.

It is "en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz" in the webpage "Populate the target and boot the image"
REF: https://wiki.st.com/stm32mpu/wiki/Getting_started/STM32MP1_boards/STM32MP157x-DK2/Let%27s_start/Populate_the_target_and_boot_the_image
It is "en.flash-stm32mp1-openstlinux-6-1-yocto-mickledore-mp1-v23-06-21.tar.gz" in the webpage "STM32MP1-Ecosystem-v5.0.0 Starter Package"
REF: https://www.st.com/en/embedded-software/stm32mp1starter.html#get-software

Hence, the command "tar xvf en.flash-stm32mp1-openstlinux-6.1-yocto-mickledore-mp1-v23.06.21.tar.gz" shown in the webpage "Populate the target and boot the image" cannot be copied, pasted, and used directly.

 

-----------------------------
[System information]
Operation system: VMware, DISTRIB_DESCRIPTION="Ubuntu 22.04.3 LTS" provided by osboxes.org
Target board: STM32MP157F-DK2
STM32CubeProgrammer version: 2.14
Ecosystem version: 5.0.0