cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-SMBUS 2.1.0 Condensed command table config parameter error

hno-wires
Associate

We are using this the X-CUBE-SMBUS middleware for a simple SMBus like device, and noticed that the generated configuration file sets the wrong define for the "Condensed command table" setting.

The generated config file sets the DENSE_CMD_TABLE define, but the library expects DENSE_CMD_TBL

X-CUBE-SMBUS/2.1.0/STM32CubeMX/templates/stm32_config_stack_h.ftl:

[#if SMB_densetable_value == "1"]
#define DENSE_CMD_TABLE
[/#if

should read

[#if SMB_densetable_value == "1"]
#define DENSE_CMD_TBL
[/#if

The error is noticeable if the PMBUS version is set to 1.1 or 1.2. Setting PMBUS version to 1.3 (default) hides the error as  DENSE_CMD_TBL is a required feature for PMBUS 1.3 and is automatically enabled regardless of what the CubeMX config says.

In our case we are using the library for a minimal SMBus like device, not using any PMBus features. So PMBUS feature level is set to 1.1 and most features are disabled.

0 REPLIES 0