cancel
Showing results for 
Search instead for 
Did you mean: 

Why does the progress bar for Copying libraries files stacks at around 65% when I try to generate code for Keil MDK using STM32CubeMX

NBlas.1
Associate

Operating System: Windows 10 Pro 64-bit (10.0, Build 17134) (17134.rs4_release.180410-1804)

                Language: English (Regional Setting: English)

     System Manufacturer: Dell Inc.

            System Model: Latitude E6430

                    BIOS: A18 (type: UEFI)

               Processor: Intel(R) Core(TM) i7-3540M CPU @ 3.00GHz (4 CPUs), ~3.0GHz

                  Memory: 4096MB RAM

     Available OS Memory: 4002MB RAM

               Page File: 4149MB used, 1260MB available

             Windows Dir: C:\WINDOWS

         DirectX Version: DirectX 12

     DX Setup Parameters: Not found

        User DPI Setting: 96 DPI (100 percent)

      System DPI Setting: 96 DPI (100 percent)

         DWM DPI Scaling: Disabled

                Miracast: Available, with HDCP

Microsoft Graphics Hybrid: Not Supported

          DxDiag Version: 10.00.17134.0001 64bit Unicode

------------

DxDiag Notes

------------

     Display Tab 1: No problems found.

       Sound Tab 1: No problems found.

         Input Tab: No problems found.

--------------------

DirectX Debug Levels

--------------------

Direct3D:   0/4 (retail)

DirectDraw: 0/4 (retail)

DirectInput: 0/5 (retail)

DirectMusic: 0/5 (retail)

DirectPlay: 0/9 (retail)

DirectSound: 0/5 (retail)

DirectShow: 0/6 (retail)

---------------

Display Devices

---------------

          Card name: Intel(R) HD Graphics 4000

       Manufacturer: Intel Corporation

          Chip type: Intel(R) HD Graphics Family

           DAC type: Internal

        Device Type: Full Device (POST)

         Device Key: Enum\PCI\VEN_8086&DEV_0166&SUBSYS_05341028&REV_09

      Device Status: 0180200A [DN_DRIVER_LOADED|DN_STARTED|DN_DISABLEABLE|DN_NT_ENUMERATOR|DN_NT_DRIVER]

 Device Problem Code: No Problem

 Driver Problem Code: Unknown

     Display Memory: 1792 MB

   Dedicated Memory: 0 MB

      Shared Memory: 1792 MB

       Current Mode: 1366 x 768 (32 bit) (40Hz)

        HDR Support: Not Supported

   Display Topology: Internal

 Display Color Space: DXGI_COLOR_SPACE_RGB_FULL_G22_NONE_P709

    Color Primaries: Red(0.640148,0.330578), Green(0.300305,0.600109), Blue(0.149914,0.060070), White Point(0.313000,0.329602)

  Display Luminance: Min Luminance = 0.500000, Max Luminance = 270.000000, MaxFullFrameLuminance = 270.000000

       Monitor Name: Generic PnP Monitor

      Monitor Model: unknown

         Monitor Id: AUO193C

        Native Mode: 1366 x 768(p) (60.067Hz)

        Output Type: Internal

Monitor Capabilities: HDR Not Supported

Display Pixel Format: DISPLAYCONFIG_PIXELFORMAT_32BPP

     Advanced Color: Not Supported

        Driver Name: igdumdim64.dll,igd10iumd64.dll,igd10iumd64.dll

 Driver File Version: 10.18.0010.4303 (English)

     Driver Version: 10.18.10.4303

        DDI Version: 11.2

     Feature Levels: 11_0,10_1,10_0,9_3,9_2,9_1

       Driver Model: WDDM 1.3

 Graphics Preemption: DMA

 Compute Preemption: Thread group

           Miracast: Supported

 Hybrid Graphics GPU: Integrated

     Power P-states: Not Supported

     Virtualization: Not Supported

         Block List: No Blocks

 Catalog Attributes: N/A

  Driver Attributes: Final Retail

   Driver Date/Size: 10/8/2015 3:00:00 AM, 11053048 bytes

        WHQL Logo'd: Yes

    WHQL Date Stamp: Unknown

  Device Identifier: {D7B78E66-4226-11CF-5763-3E25B4C2C735}

          Vendor ID: 0x8086

          Device ID: 0x0166

          SubSys ID: 0x05341028

        Revision ID: 0x0009

 Driver Strong Name: oem40.inf:5f63e5341859ec8c:iIVBM_w10:10.18.10.4303:pci\ven_8086&dev_0166

     Rank Of Driver: 00D12001

        Video Accel: ModeMPEG2_A ModeMPEG2_C ModeWMV9_C ModeVC1_C

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TDK
Super User

Clearly a program bug. It pops up here occasionally.

I think someone said deleting the Drivers folder got it to work. Might try that.

Backup your program first.

If you feel a post has answered your question, please click "Accept as Solution".