cancel
Showing results for 
Search instead for 
Did you mean: 

Why are the STM32CubeIDE - CubeMX ETH selections different between the Windows and Linux versions

GGree.1
Associate III

In the Linux version, the general Parameters Configuration window has settings for:

Ethernet MAC Address

Tx Descriptor Length

First Tx Descriptor Address

Rx Descriptor Length

First Rx Descriptor Address

Rx Buffers Length

In the Windows version, the general Parameters Configuration window has the same setting with one addition for:

RX Buffers Address

Why is that?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0