2026-05-15 10:30 AM
This software has started reporting memory issues and wanting to close every few minutes. This never used to happen until I updated to 2.0.0 and I wrote a bunch of code in a fairly large project this week. I have tried all the suggestions that I could, ending in updating to 2.1.1 and it doesn't go away.
I tried updating the memory usage to 6GB of RAM (in steps) in the file stm32cubeide.ini (-Xms and -Xmx). I deleted a bunch of folders in the /Users/xxxxx/ directory that started with .stm which worked for another person on this forum.
I can't do my work anymore. This software has become unusable! I really don't know what to do to get it back to the way it has worked for the past decade.
Any advice would be greatly appreciated. If I need to contact IT about something they might have installed on this computer that is breaking this program, I could use some direction as to what that might be.
Thanks!
Michael
2026-05-15 10:55 AM - edited 2026-05-15 10:57 AM
So why not using an older version...?
btw
I use v 1.18.1 , running fine on my LinuxMX, and 1.19.0 on Win10 .
2026-05-15 3:41 PM
I believed that staying up to date with the latest versions would offer the most reliability but...shame on me. :)
If an employee of ST can't offer anything reasonable, I might have to downgrade the software and see what happens.
2026-05-15 6:48 PM
> If I need to contact IT about something they might have installed on this computer that is breaking this program,
So your PC is a "work" machine managed by your IT? Then definitely ask them what changed recently. They could install some "security" or "compliance" stuff that is configured/updated remotely.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.