cancel
Showing results for 
Search instead for 
Did you mean: 

We have downloaded the STSW-IOD01 firmware for the Nucleo-L073rz board. The STSW-IOD01 project is not set up in a format able to be used with the STM32CubeMx. Is there some way to convert it so we can use it with the STM32CubeMx environment?

LFerg.2
Associate

We have selected the Nucleo-L073rz board in STM32CubeMx, created a project and are copying the code from STSW-IOD01 into the new project but this is very tedious and prone to errors.

Also, please note that the STSW-IOD01 firmware comes preloaded in the Nucleo-073rz board.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0