STM32L011 Temperature sensor calibration (Possible bug in library)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-05-23 8:35 AM
Hi all,
I am trying to use internal temperature sensor on Nucleo L011K4 and using macro from LL library (__LL_ADC_CALC_TEMPERATURE_TYP_PARAMS) I get complete garbage.
STM32Cube_FW_L0_V1.11.2
STM32CubeMx 5.0.1
LL libraries used, no HAL
ADC is running in DMA mode with HW oversampling by 8, 12.5 clock S&H time (should be enough for TEMP sensor) and each ADC EOS this value again averaged in SW.
When I looked closely to datasheet and reference manual I wrote my code without this macro and I still getting nonsense data out of it. I found that TS_CAL2 value from Factory Option bytes is far different than expected value, so when I used 670 constant instead - and I got something real temperature finally.
Question 1: why at production calibration value is like 1.5 times bigger than supposed to be?
Question 2: Is there a bug in LL macro? It looks like there one unnecessary multiply by 1000
Question 3: Do I need to recalibrate temp sensor at 130C or can use different temperature?
Question 4: Can I store calibration value in option bytes and how?
Question 5: Is TS_CAL1 value can be used if I calibrate it by myself? I want measure temperature using 2 points calibration.
Solved! Go to Solution.
- Labels:
-
ADC
-
STM32CubeMX
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-05-28 7:23 AM
Note that the calibration at the factory was done using Vdda=3V, but the Nucleo eval board uses Vdda=3.3V. Did you account for this difference?
Would you be able to:
- Provide the raw ADC counts that you read at room temperature
- Measure and provide the actual Vdda voltage (AREF, connector CN4, pin13)
- Provide a second measurement at a different temperature (cold or hot)
Thanks!

- « Previous
-
- 1
- 2
- Next »