cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Feature Request - Show Baud Rate error percentage for serial peripherals

It would be nice to see the baud rate's error percentage (especially for asynchronous serial peripherals) when setting the desired baud rate in the peripheral's configuration dialog.

For example, I'm setting 115200 Bits/s for USART1, STM32CubeMX knows that I have oversampling enabled, and my USART1 is clocked by PCLK2 which is 8Mhz. So it can calculate:

BRR = 8,000,000 / 115,200 = 69.44 = 69

8,000,000 / 69 = 115,942.02

(115,942.02 / 115,200) * 100 = 100.64

So the error percentage is +0.64%

Depending on the error percentage, it can also become a warning when it's too much.

Thanks!

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Amel NASRI
ST Employee

Hello,

Please note that your proposal is shared with our STM32CubeMX team, to be assessed and then let you know what can be done.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

>> it can also become a warning when it's too much.

Can't it sustain something like +/-6.25%

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..