Skip to main content
JulienD
Associate III
November 22, 2018
Question

SDMMC module does not answer used with FatFS

  • November 22, 2018
  • 2 replies
  • 686 views

Hello 

I'm testing implementation of sdcard / FatFS on F446.

First I started with the example. It works.

Now, I'm trying to implement a basic test app created from scratch with CubeMx.

I configured a simple project with fatFS, SDIO, no DMA, no OS.

int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration----------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_SDIO_SD_Init();
 MX_FATFS_Init();
 /* USER CODE BEGIN 2 */
 
 testSD();
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1) {
 
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 
 }
 /* USER CODE END 3 */
 
}
void testSD() {
 if (f_mount(&SDFatFS, (TCHAR const*) SDPath, 0) == FR_OK) {
 if (f_mkfs(SDPath, FM_ANY, 0, workBuffer, sizeof(workBuffer)) != FR_OK) {
 
 FIL file;
 if (f_open(&file, "a.txt", FA_CREATE_ALWAYS | FA_WRITE) == FR_OK) {
 uint32_t byteswritten; /* File write/read counts */
 uint8_t wtext[] = "This is STM32 working with FatFs uSD\r\n";
 f_write(&file, wtext, sizeof(wtext), (void *) &byteswritten);
 f_close(&file);
 }
 }
 }
}

With this code, is seems that the SDMMC module does not answer to any command and the first one

happens with this call stack:

SDMMC_GetCmdResp1() at stm32f4xx_ll_sdmmc.c:1 197 
SDMMC_CmdAppCommand() at stm32f4xx_ll_sdmmc.c:892 
SD_PowerON() at stm32f4xx_hal_sd.c:2 561 	
HAL_SD_InitCard() at stm32f4xx_hal_sd.c:386 
HAL_SD_Init() at stm32f4xx_hal_sd.c:335 
BSP_SD_Init() at bsp_driver_sd.c:81 
SD_initialize() at sd_diskio.c:146 
disk_initialize() at diskio.c:100 
f_mkfs() at ff.c:5 323 
initFS() at testSD.c:34 
testSD() at testSD.c:123 
main() at main.c:117 

SDMMC_GetCmdResp1() returns SDMMC_ERROR_CMD_RSP_TIMEOUT.

I did compare the configuration of my app and the example. I compared clocks, interruptions (it seems that none is used).

I also compared the calls that are made to sd or fatFS libs and I can't see the difference.

What did I miss?

If needed, ioc file is here: https://we.tl/t-6FzT0Plvh4 .

Thanks

Julien

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
November 22, 2018

Almost certainly not an issue with top level code, so focus on the low level plumbing.

Also I would not MKFS on known good formatted SD Cards.

Start at the lowest level, and have test code that only reads.

Disable Flow control.

Dump registers (RCC, SDIO) and compare/contrast working/non-working.

Surprised there would be no interrupt handler code.

Review other threads with issues using CubeMX SDIO/SDMMC, automated tools tend to break things consistently.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
JulienD
JulienDAuthor
Associate III
November 27, 2018

Pff, my bad. SD pins where not the same in the soft and hard....

Thanks for helping a mentally disabled...