Skip to main content
LMI2
Senior III
July 1, 2019
Question

Please make the pin list from CubeMX more configurable

  • July 1, 2019
  • 3 replies
  • 766 views

I have an old PCB CAD and 100 pin STM32F746 CPU. I would like to have a component symbol where pins have their functional names. Like for instance USART2_TX/PA2 instead of plain PA2.

And the list must contain every pin and be in CSV format.

This is of course what my old Pads eats, others may have different CAD SW.

Or you could make several PCB Cad formats available.

This is a sample of the file I could import

Pin Group,Number,Name,Type,Swap,Seq.

Pin Group,Number,Name,Type,Swap,Seq

Gate-A,1,RESET/PE2,Undefined,0,

Gate-A,2,GPIO_OUT/PE3,Undefined,0,

Gate-A,3,PE4,Undefined,0,

Gate-A,4,PE5,Undefined,0,

Gate-A,5,TurnOff/PE6,Undefined,0,

Gate-A,6,VBAT,Undefined,0,

Gate-A,7,PC13-ANTI_TAMP,Undefined,0,

Gate-A,8,PC14-OSC32_IN,Undefined,0,

Gate-A,9,PC15-OSC32_OUT,Undefined,0,

Gate-A,10,VSS,Undefined,0,

Gate-A,11,VDD,Undefined,0,

Gate-A,12,PH0-OSC_IN,Undefined,0,

Gate-A,13,PH1-OSC_OUT,Undefined,0,

Gate-A,14,NRST,Undefined,0,

Gate-A,15,PC0,Undefined,0,

Gate-A,16,PC1,Undefined,0,

This topic has been closed for replies.

3 replies

GSome
Visitor II
July 3, 2019

If you can read an xml file this is where cubeMX gets the information:

chip stm32F303 for example:

C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeMX\db\mcu\STM32F303Z(D-E)Tx.xml

An example of pin information:

<Pin Name="PA2" Type="I/O" Position="36">

<Signal Name="ADC1_IN3"/>

<Signal Name="ADC3_EXTI2"/>

<Signal Name="ADC4_EXTI2"/>

<Signal Name="COMP2_INM"/>

<Signal Name="COMP2_OUT"/>

<Signal Name="OPAMP1_VOUT"/>

<Signal Name="TIM15_CH1"/>

<Signal Name="TIM2_CH3"/>

<Signal Name="TSC_G1_IO3"/>

<Signal Name="USART2_TX"/>

<Signal Name="GPIO" IOModes="Input,Output,Analog,EVENTOUT,EXTI"/>

</Pin>

LMI2
LMI2Author
Senior III
July 4, 2019

Thank you. I have to check what I can do with this. Maybe copy/paste from notepad to excel. I still wish some flexibility in the documentation.

LMI2
LMI2Author
Senior III
July 7, 2019

I checked the xml file, it shows all variants which a pin can have. I need just the one I am currently using. In a full board manual editing will create errors.

<Pin Name="PD10" Type="I/O" Position="57"><Signal Name="FMC_D15"/><Signal Name="FMC_DA15"/><Signal Name="LTDC_B3"/><Signal Name="USART3_CK"/><Signal Name="GPIO" IOModes="Input,Output,Analog,EVENTOUT,EXTI"/>