2025-05-14 2:14 AM
Hello Community,
I have a Nucleo-U5A5ZJ-Q development board and have generated code for it using CubeMX (version 6.12.0). The generated code contains this for the user button:
void EXTI13_IRQHandler(void)
{
/* USER CODE BEGIN EXTI13_IRQn 0 */
/* USER CODE END EXTI13_IRQn 0 */
BSP_PB_IRQHandler(BUTTON_USER);
/* USER CODE BEGIN EXTI13_IRQn 1 */
/* USER CODE END EXTI13_IRQn 1 */
}If I enable the RNG in CubeMX and enable its global interrupt and then re-generate the code the above changes to:
void EXTI13_IRQHandler(void)
{
/* USER CODE BEGIN EXTI13_IRQn 0 */
/* USER CODE END EXTI13_IRQn 0 */
HAL_EXTI_IRQHandler(&H_EXTI_13);
/* USER CODE BEGIN EXTI13_IRQn 1 */
/* USER CODE END EXTI13_IRQn 1 */
}Which doesn't compile as H_EXTI_13 is not defined anywhere that I can see in any file. am I missing something or is this a glitch in CubeMX. If I restore line 6 to its original value then the code compiles.
Any help much appreciated.
Solved! Go to Solution.
2025-05-19 4:06 AM
Hello @DenzilDexter ,
Thank you for bringing to our attention this issue.
An internal ticket is raised to the development team (Ticket Number: 210032)
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-15 4:48 AM
Hello @DenzilDexter ,
First let me thank you for posting and welcome to the ST Community.
For more investigation, I suggest that you provide your Ioc.File.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-15 5:14 AM
Hi @DenzilDexter,
I reproduced the same example that you did and I didn't have any problems after enabling RNG.
Here is a screenshot before enabling RNG:
and her is a screenshot after enabling RNG:
I think you should update the version of CubeMx that you are using (the latest version is 6.14.1).
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-18 11:58 PM
2025-05-19 1:38 AM
Hello @DenzilDexter ,
Let me thank you for your interaction.
I am currently investigation your request and I will get back to you ASAP.
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-05-19 4:06 AM
Hello @DenzilDexter ,
Thank you for bringing to our attention this issue.
An internal ticket is raised to the development team (Ticket Number: 210032)
Thanks.
Mahmoud
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-06-11 12:14 AM
For anyone seeing the same issue here's what the result was from ST:
I have investigated the issue you reported and can confirm that it is not related to the RNG. I have been able to reproduce your issue and have observed that altering the pin state of pin PC13 from Reset_State to GPIO_EXTI13 results in the same behaviour you experienced.
Following our internal discussions, I would like to inform you that the issue you raised will be addressed in the upcoming release of STM32CubeMX, version 6.15.0.
Thanks to ST for figuring this out so quickly.