2019-10-19 9:41 AM
I downloaded all 5 mx-cube libraries for the stm32h7 series, but it says "MCU not supported" when I clip on stm32745zi?
it works with other H series.
what am I missing?
2019-10-19 12:02 PM
update: it doesn't work with any of the dual core H7s, but I can't find anything on the STM website that I haven't installed.
I'm pretty sure I'm missing something simple. l
2019-10-19 1:08 PM
Sort of figured it out. I have version 5.0.1 of mx cube when I use the IDE in Eclipse. I updated the stand-alone mx cube to the latest version and it works with the dual core, H7 so the problem is the mx-cube updating when integrated into Eclipse. I did all full update of Eclipse after installing the current version of mx cube, but Eclipse is still using the older version of mx cube and there are no available upgrades, so I think there is a bug.