2019-12-25 6:18 PM
I downloaded and installed stm32cubemx version 5.4,and the default installation configuration is maintained.When I tried to generate an MDK project, I reported an error.
But it can be used normally after uninstalling and installing version 5.3.
I don't know why?I have tried to uninstall and then reinstall, or check if there is a Chinese path and other methods, which are not available for normal use.
Help me...
I use the win10 64 bit system.
java version "1.8.0_231"
Java(TM) SE Runtime Environment (build 1.8.0_231-b11)
Java HotSpot(TM) Client VM (build 25.231-b11, mixed mode, sharing)
Solved! Go to Solution.
2019-12-25 7:04 PM
Now it's solved. It should be a Java environment configuration problem. I need to uninstall JRE again and install it again. Sorry...
2019-12-25 7:04 PM
Now it's solved. It should be a Java environment configuration problem. I need to uninstall JRE again and install it again. Sorry...
2020-02-03 11:52 PM
Uninstall the java program installed on the computer and install the current version again. It will be fine.