2019-11-15 02:37 AM
I am trying to understand whether or not I would have to get this tool approved under the medical standards we must adhere to for a class B type medical device.
The standards are
IEC 62304
ISO 13485
Solved! Go to Solution.
2019-11-17 08:57 AM
A cursory review of the forum should indicate that CubeMX fails to meet basic industry QA standards/expectation.
The parts also aren't sold into circumstance were failure, or normal usage, might result in death or injury.
You should engage with ST sales directly.
2019-11-15 04:51 AM
Please ask a vaguer question.
2019-11-17 08:31 AM
rich1 ...If you can't understand the question please just do not involve yourself.
2019-11-17 08:57 AM
A cursory review of the forum should indicate that CubeMX fails to meet basic industry QA standards/expectation.
The parts also aren't sold into circumstance were failure, or normal usage, might result in death or injury.
You should engage with ST sales directly.
2019-11-17 11:08 AM
Makes sense looking at the standard of the code generated by CubeMX. Many thanks