cancel
Showing results for 
Search instead for 
Did you mean: 

I do not know what version of CubeMx this project was made with. (eg Version 5.1.0) I also do not know what version of the firmware package it is.(eg STM32Cube FW_F1 V1.3.1)

JKim.15
Associate II

I downloaded the project (using CubeMx) from GITHUB, which was already made.

But I do not know what version of CubeMx this project was made with. (eg Version 5.1.0)

I also do not know what version of the firmware package it is.

(eg STM32Cube FW_F1 V1.3.1)

This project is a project made four months ago.

Is there anyone who can answer these two questions?

Currently, I am using the latest version of CubeMx.

Thank you. ^^

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0