cancel
Showing results for 
Search instead for 
Did you mean: 

I can't receive from uart3 and up on STM32F730R8

AKapl
Associate

I want to use circular DMA to receive data of unknown length on 4 uarts of STM32F730R8, but I receive data just on first two of them. Transmission works and I use HAL library. Code is generated by MX configuration tool and all uarts are configured identically.

HAL_UART_Receive_DMA(&huart1,readBuffer,sizeof(readBuffer));
  HAL_UART_Receive_DMA(&huart2,debgBuffer,sizeof(debgBuffer));
  HAL_UART_Receive_DMA(&huart3,Buffer1,sizeof(Buffer1));
  HAL_UART_Receive_DMA(&huart4,Buffer2,sizeof(Buffer2));
  HAL_UART_Receive_DMA(&huart6,Buffer3,sizeof(Buffer3));
 
  HAL_UART_Transmit(&huart1, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
  HAL_UART_Transmit(&huart2, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
  HAL_UART_Transmit(&huart3, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
  HAL_UART_Transmit(&huart4, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
  HAL_UART_Transmit(&huart6, (uint8_t *)&"\nHello mr. Freeman", 18, 0xFFFF);
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
	  for(int i = 0; i<sizeof(readBuffer); i++){
		  RX[i] = readBuffer[i];
		  if(RX[i] == 0xA5){
			  HAL_UART_Transmit(&huart1, (uint8_t *)&"\nWelcome to city 17", 19, 0xFFFF);
		  }
		  readBuffer[i] = 0;
	  }
	  for(int i = 0; i<sizeof(debgBuffer); i++){
		  dbgRX[i] = debgBuffer[i];
		  if(dbgRX[i] == 0xA5){
			  HAL_UART_Transmit(&huart2, (uint8_t *)&"\nWelcome to city 18", 19, 0xFFFF);
		  }
		  debgBuffer[i] = 0;
	  }
	  for(int i = 0; i<sizeof(Buffer1); i++){
		  RX1[i] = Buffer1[i];
		  if(RX1[i] == 0xA5){
			  HAL_UART_Transmit(&huart3, (uint8_t *)&"\nWelcome to city 19", 19, 0xFFFF);
		  }
		  Buffer1[i] = 0;
	  }
	  for(int i = 0; i<sizeof(Buffer2); i++){
		  RX2[i] = Buffer2[i];
		  if(RX2[i] == 0xA5){
			  HAL_UART_Transmit(&huart4, (uint8_t *)&"\nWelcome to city 20", 19, 0xFFFF);
		  }
		  Buffer2[i] = 0;
	  }
	  for(int i = 0; i<sizeof(Buffer3); i++){
		  RX3[i] = Buffer3[i];
		  if(RX3[i] == 0xA5){
			  HAL_UART_Transmit(&huart6, (uint8_t *)&"\nWelcome to city 21", 19, 0xFFFF);
		  }
		  Buffer3[i] = 0;
	  }
}
 
static void MX_DMA_Init(void) 
{
 
  /* DMA controller clock enable */
  __HAL_RCC_DMA2_CLK_ENABLE();
  __HAL_RCC_DMA1_CLK_ENABLE();
 
  /* DMA interrupt init */
  /* DMA1_Stream1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Stream1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Stream1_IRQn);
  /* DMA1_Stream2_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Stream2_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Stream2_IRQn);
  /* DMA1_Stream5_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA1_Stream5_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA1_Stream5_IRQn);
  /* DMA2_Stream1_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA2_Stream1_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA2_Stream1_IRQn);
  /* DMA2_Stream2_IRQn interrupt configuration */
  HAL_NVIC_SetPriority(DMA2_Stream2_IRQn, 0, 0);
  HAL_NVIC_EnableIRQ(DMA2_Stream2_IRQn);
 
}

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

Polled Rx works?

Read out and check/post content of relevant USART and DMA registers.

JW