cancel
Showing results for 
Search instead for 
Did you mean: 

I am working with STM32F407VGt6-DISC1, I am facing a problem in getting LSE clock frequency out of MCO1 pin, and also other external source of clock whereas the same process for internal clock measurement through i worked fined.

VChou.1
Associate

Here i attached my main.c file.

and

When I run my debugger , i see that my program is stucked in error handler

//////////

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

//////////

And for measuring internal clock sources such as HSI, HSE. it worked fine but whenever i include LSE source :it stuck in error_handler

///////////////

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_HSE

|RCC_OSCILLATORTYPE_LSE;

//////

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User

The 32.768kHz crystal is not mounted on the F4-DISCO by default, did you get one? You need also to add the related capacitors and disconnect/connect some solder bridges according to the DISCO's User Manual.

JW