2026-03-12 8:22 PM - last edited on 2026-03-12 9:15 PM by Imen.D
안녕하세요 STM32N6570-DK의 사용하기 위한 cubemx 설정이 필요합니다. 카메라, lcd, sd카드, usb, eth 등 기능을 다 살린 cubemx 설정 또는 ioc 파일을 받고 싶습니다. 확인 부탁 드립니다.
Hello, I need a cubemx setting for use of STM32N6570-DK. I would like to receive a cubemx setting or an ioc file that utilizes all the functions such as camera, lcd, sd card, usb, eth, etc. Please check it.
2026-03-12 9:24 PM
While creating new project you can directly select your Eval board with all its peripheral initialize.
2026-03-12 9:46 PM
If you select a dk board from cubemx, it loses a few features and doesn't do the exact action.
2026-03-13 5:48 AM
What features does it lose?
2026-03-17 6:53 PM
Example In DCMIPP_Continuous Mode, there is no CUBEMX setting data.