cancel
Showing results for 
Search instead for 
Did you mean: 

Getting errors after including arm_math.h

RShar.9
Senior

Hello i want to use dsp in my project in Keil IDE for that i have to include arm_math.h.

In that case i am getting 30 errors

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1183): error: #79: expected a type specifier

  __STATIC_FORCEINLINE int32_t __SMMLA(

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1183): error: #101: "int32_t" has already been declared in the current scope

  __STATIC_FORCEINLINE int32_t __SMMLA(

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1183): error: #141-D: unnamed prototyped parameters not allowed when body is present

  __STATIC_FORCEINLINE int32_t __SMMLA(

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1188): error: #20: identifier "sum" is undefined

   return (sum + (int32_t) (((int64_t) x * y) >> 32));

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1188): error: #20: identifier "x" is undefined

   return (sum + (int32_t) (((int64_t) x * y) >> 32));

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1188): error: #20: identifier "y" is undefined

   return (sum + (int32_t) (((int64_t) x * y) >> 32));

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1801): error: #757: function "int32_t" is not a type name

     int32_t shift,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1816): error: #757: function "int32_t" is not a type name

     int32_t shift,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1914): error: #757: function "int32_t" is not a type name

     int32_t resetStateFlag);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1932): error: #757: function "int32_t" is not a type name

     int32_t resetStateFlag);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1951): error: #757: function "int32_t" is not a type name

     int32_t resetStateFlag);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4585): error: #757: function "int32_t" is not a type name

      int32_t *pTapDelay;      /**< points to the array of delay values. The array is of length numTaps. */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4598): error: #757: function "int32_t" is not a type name

      int32_t *pTapDelay;      /**< points to the array of delay values. The array is of length numTaps. */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4611): error: #757: function "int32_t" is not a type name

      int32_t *pTapDelay;      /**< points to the array of delay values. The array is of length numTaps. */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4624): error: #757: function "int32_t" is not a type name

      int32_t *pTapDelay;      /**< points to the array of delay values. The array is of length numTaps. */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4659): error: #757: function "int32_t" is not a type name

     int32_t * pTapDelay,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4695): error: #757: function "int32_t" is not a type name

     int32_t * pTapDelay,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4733): error: #757: function "int32_t" is not a type name

     int32_t * pTapDelay,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(4771): error: #757: function "int32_t" is not a type name

     int32_t * pTapDelay,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5544): warning: #174-D: expression has no effect

   int32_t i;                  /* Index variable */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5544): error: #65: expected a ";"

   int32_t i;                  /* Index variable */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5548): error: #20: identifier "i" is undefined

   i = (int32_t) ((x - S->x1) / xSpacing);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5601): warning: #174-D: expression has no effect

   int32_t index;                /* Index to read nearest output values */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5601): error: #65: expected a ";"

   int32_t index;                /* Index to read nearest output values */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5606): error: #20: identifier "index" is undefined

   index = ((x & (q31_t)0xFFF00000) >> 20);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5659): warning: #174-D: expression has no effect

   int32_t index;                /* Index to read nearest output values */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5659): error: #65: expected a ";"

   int32_t index;                /* Index to read nearest output values */

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5664): error: #20: identifier "index" is undefined

   index = ((x & (int32_t)0xFFF00000) >> 20);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5664): error: #31: expression must have integral type

   index = ((x & (int32_t)0xFFF00000) >> 20);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5664): error: #18: expected a ")"

   index = ((x & (int32_t)0xFFF00000) >> 20);

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5940): error: #757: function "int32_t" is not a type name

  int32_t * circBuffer,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5941): error: #757: function "int32_t" is not a type name

  int32_t L,

C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(5943): error: #757: function "int32_t" is not a type name

is there any special thing to do for including arm_math.h

1 ACCEPTED SOLUTION

Accepted Solutions

hello, when i included arm_math.h from keil it's taking different path

when i generated program from cubemx that time select copy_all_used_libraries_into_the_project in project manager then it will generate dsp header files into my project than i include that arm_math.h header file from project_name/Drivers/CMSIS/DSP/Include path.

and give that include path in c/c++ project

than it will work

View solution in original post

11 REPLIES 11

Probably need to be including other libraries first. Try stdint.h

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

stdint.h not working

I tried many things but when ever i add arm_math.h header file to use DSP function many errors came out, i am sharing my project to you if u want you can check it and try to resolve it. Please

Ozone
Lead III

> In that case i am getting 30 errors

Always start with the first listed error. Some cause a loooong list of aftereffects.

> C:\Keil_v5\ARM\PACK\ARM\CMSIS\5.6.0\CMSIS\DSP\Include\arm_math.h(1183): error: #79: expected a type specifier  __STATIC_FORCEINLINE int32_t __SMMLA(

Check for toolchain-specific "# ifdef"s before.

Check where typedef'd specifiers or qualifiers like __STATIC_FORCEINLINE are defined, and how they are included.

Tilen MAJERLE
ST Employee

Please check if you have ARM_MATH_CMx defined in your Keil project (under settings ->C/C++ -> Defines), where x is a number of your Cortex.

Edit: I see now you have STM32H7 in Keil, and you have these defines:

USE_HAL_DRIVER,STM32H743xx,USE_HAL_DRIVER,STM32H743xx

Should be:

USE_HAL_DRIVER,STM32H743xx,USE_HAL_DRIVER,STM32H743xx,ARM_CORTEX_CM7

Hello thanks for reply i tried both of things

defined ARM_MATH_CM7

USE_HAL_DRIVER,STM32H743xx,USE_HAL_DRIVER,STM32H743xx,ARM_CORTEX_CM7

but there is no effects on errors

RShar.9
Senior

Thanks it resolved

Could you please update what was the issue & solution?

Thanks, Tilen