Question
FreeRTOS Tasks stack size on STM32L4
Hi all,
I am working on stm32l486 chip.
When I created (using CubeMx) two tasks with a stack size equal to 256 words. The project is running well:
osThreadDef(Task1, vTask1, osPriorityNormal, 0, 256);
Task1Handle = osThreadCreate(osThread(Task1), NULL);
osThreadDef(Task2, vTask2, osPriorityNormal, 0, 256);
Task2Handle = osThreadCreate(osThread(Task2), NULL);The problem appears when I added a third task with a stack size equal to 256:
osThreadDef(Task3, vTask3, osPriorityNormal, 0, 256);
Task3Handle = osThreadCreate(osThread(Task3), NULL);If I reduce the stack size of each Task to 128, the problem disappear.
Why I can't use 3 tasks with a stack size equal to 256 for each task ?