2021-03-05 3:54 AM
Using Cube IDE. Generated a fresh project for a stm32f446ve target.
Activated with CubeMX uinder I2C a port with "SMBUS-two-wire-interface".
Then, without doing nothing more i have builded the configuration and flashed to target.
as soon as i start the mcu, it goes to hardfault.
Further investigation led to a DIVISION_BY_ZERO during SMSUS peripheral initialization (HAL_SMBUS_Init(&hsmbus1) ).
The division by zero arise when doing :
MODIFY_REG(hsmbus->Instance->CCR, (I2C_CCR_FS | I2C_CCR_DUTY | I2C_CCR_CCR), SMBUS_SPEED_STANDARD(pclk1, hsmbus->Init.ClockSpeed));hsmbus->Init.ClockSpeed is not set, nor in the cube-mx i have the entry to input it.
Is that a bug or i am not using correctly that ?
i was succesfull in interfacing a fuel gauge with an F3 (STM32F302) mcu and HAL.
thanks !
2021-03-09 7:03 AM
Hi @MBran.3 ,
You are right; ClockSpeed initialization is missing.
This parameter needs to be > 0 and <= 100000.
If you enable the Assert check, you will get an assert error when checking the value of this parameter in HAL_SMBUS_Init before trying to modify registers.
This is highlighted to STM32CubeMX team who will take care to provide a fix. Thanks for reporting this issue.
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.