cancel
Showing results for 
Search instead for 
Did you mean: 

Does cubeMX have the correct AXI / AHB limits for STM32H750?

JSchl.8
Associate

Hi,

Looking at the block diagram in the datasheet, ABH1, AHB2, AHB3, AHB4, AXI are listed as supporting 200MHz.

Cube (v5.0.0, H7 v1.3.0) however will not allow them to be set higher than 100 MHz, and says the must be <- 100MHz in the hover text.

Is cube or the datasheet correct?

Thanks,

Jacob

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
JSchl.8
Associate

Nevermind, didn't realize they need to be 1/2 the core speed. It lets me do 200MHz if the core is 400 MHz.

Everything is fine : )

View solution in original post

1 REPLY 1
JSchl.8
Associate

Nevermind, didn't realize they need to be 1/2 the core speed. It lets me do 200MHz if the core is 400 MHz.

Everything is fine : )