2019-10-16 4:58 PM
Dear experts,
I'm new to M7 (and H7) so pardon me for a stupid question.
Created a new .ioc file in CubeMX 5.3.0 for STM32H753 EVAL2 board.
There I can select debug interface as JTAG 5 pins or Serial wire (at least).
From the Cube report file, in Serial Wire mode it uses 2 pins:
PA14 SWCLK
PA13 SWDIO
Where is SWO ? It should be PB3, but the report file does not mention it.
In JTAG 5 pins mode it uses
PA14, PA15, PA13, PB3, PB4.
Now, in a .ioc file made by my hardware engineer, for a custom board with same MCU,
the debug mode is JTAG 5 pins.
But I cannot change it to Serial wire or even to Disabled.
Any reason, why?
None of these 5 pins are hmm... pinned.
Serial mode uses two (or three?) of JTAG 5 pins, so it should be possible to reuse them?
Is the JTAG config locked by some other component or mode selection?
Or can it be a "feature" of the Cube ?
We both have Cube 5.3.0 on Linux, Ubuntu,
Thanks in advance
Pavel A.
Solved! Go to Solution.
2019-10-16 8:35 PM
Boundary scan needs a lot of detail to execute properly, I worked with guys that build JTAG tools, schematic/net-list post-processing tools, and such.
You'd need JTAG to talk to multiple STM32 in a chain, or chained with FPGA/CPLD.
We've used it in the past to check boards, pin-to-pin continuity, etc.
2019-10-16 5:19 PM
Well TDO/SWO on PB3 does work, the plumbing is more complicated as you need to configure which MCU connects up.
You're persistent in the face of much brokenness. I don't think much of CubeMX gets tested in real-world situations, and definitely not with any rigor.
Full JTAG at least permits boundary scan, and you can chain in other components. Unless you're completely bereft of pins I would avoid committing them,
2019-10-16 6:44 PM
Clive,
Do you recommend JTAG mode over SWD for H7?
I've used only SWD mode before with F4, F0 and various ST-LINKs
Is boundary scan useful for the STM32 at all?
Thank you.
-- pa
2019-10-16 8:35 PM
Boundary scan needs a lot of detail to execute properly, I worked with guys that build JTAG tools, schematic/net-list post-processing tools, and such.
You'd need JTAG to talk to multiple STM32 in a chain, or chained with FPGA/CPLD.
We've used it in the past to check boards, pin-to-pin continuity, etc.