cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX v4.20.1 LwIP project generation for SW4STM32

Sungjune Lee
Associate
Posted on April 20, 2017 at 13:02

Hi,

I'm wondering that when CubeMX generates LwIP projects, it may be pointing wrong directories for the header files. For example, it generates list of following directories:

Middlewares/Third_Party/FreeRTOS/LwIP/src/include/lwip

Middlewares/Third_Party/FreeRTOS/LwIP/src/include/netif

Middlewares/Third_Party/FreeRTOS/LwIP/src/include/posix

whereas what is actually necessary is a single directory

Middlewares/Third_Party/FreeRTOS/LwIP/src/include

according to the source files. The same thing goes with

Middlewares/Third_Party/FreeRTOS/LwIP/system/arch

Middlewares/Third_Party/FreeRTOS/LwIP/system/OS

instead of

Middlewares/Third_Party/FreeRTOS/LwIP/system

I only use the .cproject file to convert it into Makefile. So I'm not 100% sure.

Thanks,

#cubemx #cubemx-4.20
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0