2016-05-30 12:28 PM
Hello again,
yesterday I updated to the newest version of CubeMX (v4.15.0) and since then in my project the clocks for the SDMMC and the STM32F746ZGT are disabled. In the pinout I selected the 4-Bit wide mode but the clocks are still off. I tested it with a new project -> same result. In my VM I have an old v4.9.0 and in this version the clocks still working as expected. Please can someone help? Is it a real bug?
EDIT: STM32F779 is still working on both SDMMC interfaces. The clock are enabled after I choose one of the configuration in the pinout tab. #bug #cubemx #stm32f7
2016-05-31 02:39 AM
Hi debegr,
It is already reported to our CubeMx team as an issue in the new version. Thanks for the feedback. -Hannibal-2016-06-13 11:46 PM
Dear user,
Thank you for reporting this issue. It shall be fixed within STM32CubeMX 4.16 release. Best regards.