2024-08-17 8:21 AM
2024-08-17 12:15 PM - edited 2024-08-17 12:16 PM
Bonjour @mwalt.3
Even if you set the data direction to receive only, you still need both pins on the STM32CubeMX. The only way to use just 1 pin is to set the mode to half duplex and set data direction to receive only. This will keep only 1 pin (the TX pin will do both TX and RX).
Best Regards.
STTwo-32
Best Regards.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.