cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX feature request

Daniel Hassanian
Associate III
Posted on December 02, 2017 at 10:36

Hello,

CubeMX is a good software but there are many things it's still missing, it'd be very neat to have these options implemented:

1- A Timer calculator similar to the external tool by mikroelectronika but for all MCUs and for all Timer modes.

for example i just want a timer to count a limited time(without interrupts) but i have to read the datasheet just for that.

it could be as simple as what we have for SPI clock or just more advanced to have all the option illustrated with a simple text(or GUI)

2- All peripherals could benefit a description section which can be modified inside CubeMX.(for example just to comment what that specific timer is used).

3- in Clock Configuration window it would be very nice to have the option to know which peripherals are connected to which APB bus. currently it shows some of them and for example for timers we need to read the datasheet.

4- datasheet specifies we can have peripheral to peripheral DMA requests , why don't we have that in CubeMX?

5- for FreeRTOS , it would be nice to have the option to choose the final generated code should use the cmsis port or just pure FreeRTOS functions.

Finally in the help menu there's a mistype. 'Docs & Ressources' -> 'Docs & Resources'.

#feature-request #cubemx
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
john doe
Lead
Posted on December 02, 2017 at 13:30

put the OK/Cancel buttons back in the board/chip choice pane, or if you're not willing to do that, at least let it respond to return/enter and escape to make choices.  and read up on the human interface guidelines.

Daniel Hassanian
Associate III
Posted on December 02, 2017 at 18:48

Another option which is a must have in near future is the option to generate a c++ project using HAL c codes.

Also it would be a big step if the Cube team could provide a Community library for developers to share their codes for different MCUs.