cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX feature lost when integration with CubeIDE?

Peter Allnutt
Associate III

In the old standalone version of CubeMX one could access the datasheet/application notes appropriate to the board/CPU part your project was based on.

Probably me being a bit dense but I can't see to find this in CubeIDE. Does an equivalent exist?

Used to save a lot of time hunting for relevant documents.

Thanks

Pete

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Cartu38 OpenDev
Lead III

File > New STM32 Project

Let's select your device (mcu or board) then rely on dedicated button on same target selector page to get related doc.​

berendi
Principal

Having to start a new project each time instead of just pressing Alt-D is a terrible workaround.

Cartu38 OpenDev
Lead III

Yes i may agree but at least doing the job.​

Peter Allnutt
Associate III

Thanks for the pointer, a bit of a kludge but better than nothing :) Be nice if the feature was extended in to a existing project though.